Company profile
The products
ROLLON is an international
Group that works since 1975 in the linear motion field.
ROLLON has developed
many families of products capable of solving a great number
of problems in machine design and mechanical fields, or wherever
there is the need to move machine parts using a low coefficient
of friction.
All the main families (COMPACT
RAIL, TELESCOPIC
RAIL, EASY
RAIL, UNILINE,
ECOLINE, CURVILINE,
LIGHT RAIL, X RAIL, MONO RAIL,)
offer standardized and modular solutions, made with economy
of scale which yields the best price/performance ratio.
The biggest added value is given by the ability to personalize
the product according to the application so that, if needed,
the product becomes 'unique for each customer'.
Most of the ROLLON products
are based on the general principle that makes up the essence
and originality of the ROLLON
philosophy: a C-shaped rail with internal raceways where,
depending on the application, different types of sliders can
move.
This design principle is very important in order to understand
the main advantage of the ROLLON
components compared to other linear solutions on the market:
well protected internal raceways and extremely compact rail
and slider assembly for tight space restrictions.
The structure
The Group's Corporate Headquarters is ROLLON
S.p.A. in Italy (Vimercate, Milan area).
ROLLON in rest of Europe
is directly present in Germany, Holland, Czech Republic and France.
In North America, ROLLON's
headquarters are in New Jersey, USA.
ROLLON is also present
worldwide with a network of distributors in nearly all industrialized
countries.
Quality
The company's philosophy about quality is to always provide
very reliable products and services that exceed the customer's
needs and expectations.
To confirm ROLLON's dedication
to high quality, ROLLON
has been ISO9001 - 1994 certified since 1995.
During 2001 ROLLON has
been recertified following the new standards ISO9001-2000, better known as Vision 2000.
|