slogan Rollon
logo Rollon

APPLICATIONS EXAMPLES

 

Automatic pharmacy shelf system

Compact Rail

Speed, precision and noiseless operation of the sliders are convincing arguments for using Compact Rail in this automatic pharmacy shelf system. Also the telescopic roller rail is ideal for this type of application.

 

Application example 2

Telescopic Rail DMS63

DMS63 heavy duty telescopic rails assist film roll changing. The reeling unit in a laminating system is pulled out for this purpose – in this case in a furniture industry application. This is ergonomic and safe. The telescopic rails must be able to resist the heavy weight of the rolls.

 

ASN in autoambulanza

ASN

A Medevac unit for safely transporting patients in armoured container vehicles. The close-up shows a horizontal telescopic arm in the upper stretcher. An ASN partial extraction can be seen in the front left. This does not sag even under maximum permanent load. The up and down movement of the stretcher takes place when the telescopic arms are extended – guided by Compact Rails.

 

Lettore ad ultravioletti

Compact Rail T+U

Compact Rail used in the housing of a UV Setter. The combination of K and U profiles compensates for parallelity deviations and guarantees safe operation.

rollon logo

Linear motion components