Thursday 4 September 2025
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
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
4 September 2025
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
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
Automating a production line for the transport and machining of electrical wires

Case Study

A high-tech company specialized in the design and production of electrical wires and connectors needed a customised curvilinear handling system to transport coils of electric wires through nine processing stations. The choice fell on Rollon® Nadella AXNRQ circular system in ring configuration.

With the continuous global rise of automated production systems, manufacturing companies face the challenge of integrating automation to maintain a competitive edge. Automation not only enhances efficiency but also improves flexibility, allowing plants to adapt quickly to new product designs and changing production demands. Moreover, automation reduces human error and ensures consistent product quality, making it a crucial investment for modern manufacturing facilities.

The challenge

A high-tech company specialized in the design and production of electrical wires and connectors needed an advanced automation solution to streamline its production process. Specifically, the company required a customized curvilinear handling system to transport coils of electric wires through nine machining stations while maintaining a cycle time of under two seconds between each stage.

Additionally, the system had to meet two other critical requirements: sufficient load capacity to handle coils of varying weights (8, 10, or 12 kg) and the ability to be installed on a 10-meter-long support structure already present inside the manufacturing plant.

With industrial automation playing an increasingly vital role in enhancing efficiency, flexibility, and product quality, finding a solution that optimized space, reduced manual intervention, and ensured high-speed operation was essential.

Automating Production Line Electrical Wires

AXNRQ Application example

The solution

After a thorough analysis of the application requirements, Rollon Nadella engineers proposed the AXNRQ circular system in ring configuration. This solution was selected due to its ability to meet the key operational demands of the project, offering:

  • High load capacity with robust guide rollers that support loads in all directions, helping ensure smooth and stable transportation of coils.
  • Optimized acceleration and speed, meeting the stringent stroke time requirement between machining stations.
  • Space-efficient design, allowing seamless integration onto the existing 10-meter-long support structure within the plant.

The system provided features a 10-meter-long circular track equipped with 24 carriages, ensuring continuous operation across all machining stations. Furthermore, to enhance reliability and minimize maintenance efforts, the solution includes an automatic lubrication system that helps ensure optimal performance over extended operational cycles.

Automating Production Line Electrical Wires

10-meter-long AXNRQ Circular System

The AXNRQ circular system delivers a fully integrated, ready-to-use circuit that allows manufacturers to achieve the desired performance while reducing footprint and engineering time. The core components of the system include:

  • Aluminum base for lightweight strength and easy installation.
  • Guide rails and carriages for precise and smooth movement.
  • Transmission system with gearbox and toothed belt for efficient motion control.
  • Lubrication units for extended durability and reduced maintenance.
  • Carriage indexing system to ensure accurate positioning at each processing station.
Automating Production Line Electrical Wires: Automatic Lubrication System

The automatic lubrication system

Automating Production Line Electrical Wires: the drive pulley directly mounted on the gearbox output shaft

The drive pulley directly mounted on the gearbox output shaft

The results

The implementation of the AXNRQ circular system has brought several benefits to the customer’s production process:

  • Improved motion control: the guide rollers contribute to stable and precise movement, helping to achieve accurate positioning of the coils.
  • Efficient use of space: The machined aluminum alloy base, directly connected to the gearbox, supports a compact and easy-to-install system.
  • Adaptability to specific needs: The modular and configurable design allows for a tailored approach to different production setups, potentially reducing installation time and engineering effort.

By adopting Rollon Nadella’s AXNRQ circular system, the company was able to implement an automation solution that aligns with its operational requirements, supporting efficiency and productivity improvements while optimizing the use of available space.

For more information on Rollon’s linear motion solutions and to connect with Rollon application engineers in your area or region, please get in touch with us.

Get in touch with us

Related product line

Select a product to learn more

AXNR

2
Precision linear motion solution that combines flexibility and ease of installation for linear motion circuits. Equipped with recirculating ball bearings to support high loads, even in the most demanding environments. Circular systems reduce working areas compared to traditional lines, increase efficiency and reliability and are available in two different configurations and with a variety of options.
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
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
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
Report How To Choose The Right Telescopic Bearing
Report Telescopic rail for railway and vehicle applications
White paper Rollon Linear Guides for the Train Industry
Whitepaper Anticorrosive Coatings Protect Train Components
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
Report How To Choose The Right Telescopic Bearing
Application Note Self-Aligning Linear Guides For Aircraft Seating
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
Application Note Showering Guests with Luxury
Application Note Retail Expansion Demands Unique Motion Control Solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Report Telescopic rail for railway and vehicle applications
Application Note Linear Bearing System Adds Critical Extra Space to Mobile Hospital Design
Report Linear Guide Alternatives
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Tech Talks Cleanroom-ready linear motion, engineered for precision
White paper Choosing linear motion components for medical equipment
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Report Linear movement in the pharmaceutical and medical industry: the seventh axis for clean rooms
Tech Talks Cleanroom-ready linear motion, engineered for precision
Case Study High-tech distributor taps Rollon for electronics machine
Case Study How Rollon actuators helped a Korean multinational corporation automate its battery cell manufacturing process
White paper Applications for industrial grade telescopic rails
Case Study CNC Solutions and Rollon: Advancing robotic automation for heavy-duty applications
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Report Monorail linear guide for high-load applications
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges