Thursday 4 September 2025
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
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
4 September 2025
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
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
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines

Case Study

South Korea’s automotive industry is one of the most advanced globally, recognized for its innovation, production efficiency, and robust export capabilities. This strong industrial foundation has supported the development of cutting-edge suppliers across the entire value chain. Among these is Sangsin ENG, a company that has emerged as a key automation partner for automotive manufacturing facilities in the region.

Founded in 1991, Sangsin ENG entered into an M&A (Merger and Acquisition) with Sangsin Brake Group in 2006. Sangsin ENG has since experienced significant growth, specializing in the design and manufacture of equipment for brake pad production lines. Its focus on automation and precision engineering has positioned it at the forefront of this sector.

The challenge

As part of a new project for one of its customers, Sangsin ENG needed to complete an automated production line for brake pads. The requirement was for a linear motion system capable of performing reliable pick-and-place operations and transporting components across multiple workstations within the line.

The operating environment posed particular challenges: it demanded a high standard of cleanliness while simultaneously exposing components to contaminants generated during the production process. Additionally, the system needed to deliver smooth, quiet, and fast motion to align with the customer’s production speed and requirements.

To meet these demands, Sangsin ENG turned to S.R. Tec, Rollon’s official distributor in South Korea, for a solution that could combine performance, reliability, and compatibility with the production environment.

The solution

Rollon, in collaboration with S.R. Tec, engineered a tailored solution comprising a YZ gantry system based on Speedy Rail actuators and a Robot Transfer Unit (RTU) constructed with two ELM actuators. This integrated system was installed across the entire brake pad production line, managing the full range of component handling and transfer operations with precision and consistency.

The YZ gantry was specifically designed to handle vertical and horizontal manipulation with strokes of 6,500 mm on the Y-axis and 800 mm on the Z-axis. Both axes utilize Speedy Rail SAB self-supporting actuators driven by belt system. These actuators are characterized by their deep hard-anodized surface treatment and polyamide-coated rollers, which provide high load capacity while requiring no lubrication or maintenance. Their construction also ensures robust resistance to dirt and contaminants – an essential feature for the operating conditions required by Sangsin ENG.

Complementing the gantry, the RTU enables horizontal movement along a stroke of 3,600 mm. Built with two ELM actuators, the unit features extruded and anodized aluminium profiles and a polyurethane sealing strip. This design offers complete protection of the belt drive and guide system, shielding the internal mechanisms from dust and other production debris while supporting long-term operational reliability.

Brake pad production automation system at Sangsin ENG

The YZ gantry system based on Speedy Rail actuators and a Robot Transfer Unit (RTU) with two ELM actuators supplied by Rollon. © Sangsin ENG

Performance and results

“The design approach was guided by a clear technical constraint: avoid the use of lubricants to maintain production cleanliness, while still withstanding the abrasive effects of contaminants. The selected combination of Speedy Rail and ELM actuators proved to be ideally suited for this type of demanding environment”, explains Yuji Hayashi, APAC Sales Manager Actuators Business Unit at Rollon.

For Sangsin ENG, the switch to Rollon represented a clear improvement over previous solutions: “Before using Rollon, we had developed an in-house system, but it didn’t meet our performance expectations,” explains Jaekook Bae, Managing Director at Sangsin ENG. “Two years ago, we started to use Rollon’s products. Cleanliness is critical for us. With Rollon, we don’t need grease, which is a huge benefit for the production environment. Maintenance has become easier, and the motion is fast and silent – important factors for our operations.”

Rollon’s commitment to customer support was also instrumental in the project’s success. “We initially encountered some vibration issues,” says Walter Gobbi, Sales Director APAC at Rollon. “But we responded quickly with a corrective solution and supported Sangsin throughout the process.”

”A particularly notable system resilience occurred during machine testing, when a collision damaged several components on the production line. Remarkably, Rollon’s system remained completely unaffected.” said Jaekook Bae.

“This incident demonstrated that our sizing includes a sufficient safety factor, and confirmed the reliability of our design,” adds Hayashi.

Brake pad production automation - The team

The Sangsin ENG and S.R. Tec teams with Yuji Hayashi from Rollon (third from the right). © Rollon

Looking ahead

With an eye toward expanding its footprint in the European market, Sangsin ENG is now seeking reliable partners who can help support this growth. Rollon is positioned to play a key role in this journey.

“Our customers appreciate the technical quality and cleanliness that Rollon systems guarantee. This gives us the confidence to continue our cooperation and to rely on Rollon as we grow in new markets”, concludes Jaekook Bae.

Interested in learning more about our automation solutions or starting a new project together?

Connect with Us

Related product line

Select a product to learn more

Clean-Room-Linear-ActuatorSpeedy-Rail-SAR-Belt-driven-actuatorECO-System-Belt-driven-linear-actuatorTelescopic Linear ActuatorUniline-A-Belt-driven-Linear-ActuatorModline-MCH-Belt-driven-linear-actuator

Belt driven linear actuators

22
Rollon belt driven linear actuators combine performance, strength and versatility. Ideal for harsh environments and limited space, they offer high speed and precision, with steel re-enforced driving belts.

YZ Multi-Axis (Aluminium)

9
Versatile multi-axis systems designed starting from your specific needs.
RTU - Rack & PinionRTU - Sealed BeltRTU - Open Belt

RTU (Aluminium)

3
Belt and rack and pinion driven shuttle system for moving with high dynamics every model of robot, from the smallest cobot, to the largest robot.
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
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
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
Report How To Choose The Right Telescopic Bearing
Report Telescopic rail for railway and vehicle applications
White paper Rollon Linear Guides for the Train Industry
Whitepaper Anticorrosive Coatings Protect Train Components
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
Report How To Choose The Right Telescopic Bearing
Application Note Self-Aligning Linear Guides For Aircraft Seating
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
Application Note Showering Guests with Luxury
Application Note Retail Expansion Demands Unique Motion Control Solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Report Telescopic rail for railway and vehicle applications
Application Note Linear Bearing System Adds Critical Extra Space to Mobile Hospital Design
Report Linear Guide Alternatives
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Tech Talks Cleanroom-ready linear motion, engineered for precision
White paper Choosing linear motion components for medical equipment
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Report Linear movement in the pharmaceutical and medical industry: the seventh axis for clean rooms
Tech Talks Cleanroom-ready linear motion, engineered for precision
Case Study High-tech distributor taps Rollon for electronics machine
Case Study How Rollon actuators helped a Korean multinational corporation automate its battery cell manufacturing process
White paper Applications for industrial grade telescopic rails
Case Study CNC Solutions and Rollon: Advancing robotic automation for heavy-duty applications
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Report Monorail linear guide for high-load applications
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges