Tuesday 5 August 2025
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
Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle

Case Study

Techno Agility, a company specializing in the production of vehicles for people with disabilities, partnered with Nadella—part of Rollon by Timken—to equip a special vehicle that enables Paralympic athlete Mauro Tomasi to access and drive it independently.

“We consider ourselves mobility consultants,” explains Thierry Biz, owner of Techno Agility. “Our goal is to help people by applying our knowledge to find the best solutions for their specific needs. The devices we install must genuinely improve quality of life. That’s why we strongly believe that, as far as possible, technology should adapt to people—not the other way around. We actively involve our clients at every stage of the project to clearly understand their needs and identify the most comfortable and functional driving system for them, striving to strike the best balance between human and technological requirements.”

The challenge

The project required lightweight yet robust components to support a system that would allow Mauro—who is paralysed from the waist down and has no mobility in his left arm—to access the driver’s seat directly from his wheelchair via a lifting platform installed in the rear of the vehicle. From there, he can drive independently using a joystick control system.

The equipment, installed on a specially modified Mercedes Sprinter van, was designed not only to provide paraplegic drivers with full autonomy, but also to ensure that people without disabilities can drive the vehicle safely and comfortably.

“The key message I like to share with customers,” Biz adds, “is that these systems are made for people with disabilities, but they offer a smooth and enjoyable driving experience for everyone. It’s a new way of approaching these challenges.”

To bring this vision to life, Techno Agility collaborated closely with Nadella.

The solution

Nadella engineers supported the project from initial design to final commissioning, working to identify and supply the most suitable linear motion system to meet Techno Agility’s functional and structural requirements.

The chosen solution is a 2D multi-axis system made up of two belt-driven linear units from the CLS series for the X-axis, and a rack-and-pinion linear unit for the Y-axis, all equipped with planetary gearboxes. Movement is powered by 24-volt motors, which draw energy from an auxiliary battery—ensuring the main vehicle battery remains unaffected.

Custom linear motion solution for Paralympic athlete

The multi-axis system installed on the vehicle.

The system is integrated into an internal frame, the Rollbar, which safely supports and moves a person weighing up to 150 kg within the vehicle. The structural profiles were specifically designed to ensure not only the system’s reliability, but also the consistency of motion over time. Each component was selected based on the quality of materials and in-house manufacturing processes, with quality checks at every stage—from production to final assembly.

As with all Techno Agility equipment, the entire system was tested and certified by an external authority.

Results

This solution marks a significant step toward independence for Mauro Tomasi. With a simple joystick, he can now enter his vehicle and move into the driver’s seat completely on his own. The system is fast, quiet, and compact, having no negative impact on the vehicle’s internal space.

“The key factors in choosing this linear solution were quality and reliability,” note the engineers at Rollon Nadella. “We’re proud to design systems that can make life easier for everyone—without exception.”

Who is Mauro Tomasi

On August 15, 2000, Mauro Tomasi was involved in a serious motorbike accident that left him paralysed from the waist down and without use of his left arm. Since 2012, when he participated in his first race—the International Lake Marathon—he has taken part in more than 100 sporting events, completing over 70 marathons, including the New York City Marathon in 2014. In 2023 alone, he covered 10,335 kilometers. All of the races Mauro competes in are what he calls “Endeavours” (Imprese). Remarkably, he does not use racing wheelchairs or hand bikes but instead pushes himself using his everyday wheelchair—driven by one arm. “Limits exist only in our minds,” Mauro says. “And often, they’re created by others.”

Mauro Tomasi at the Athens Marathon

To find out more about Rollon Group’s linear motion solutions, please contact us.

Contact us

Related product line

Select a product to learn more

Clean-Room-Linear-ActuatorSpeedy-Rail-SAR-Belt-driven-actuatorECO-System-Belt-driven-linear-actuatorTelescopic Linear ActuatorUniline-A-Belt-driven-Linear-ActuatorModline-MCH-Belt-driven-linear-actuator

Belt driven linear actuators

22
Rollon belt driven linear actuators combine performance, strength and versatility. Ideal for harsh environments and limited space, they offer high speed and precision, with steel re-enforced driving belts.
Rack-and-pinion-driven-linear-actuatorstelescopic-system-tls.png

Rack and pinion driven linear actuators

4
Rack-and-pinion driven actuators in the Rollon range offer an excellent balance of payload, precision and durability, ideal for applications requiring long strokes linear motion.

YZ Multi-Axis (Aluminium)

9
Versatile multi-axis systems designed starting from your specific needs.
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
Report How To Choose The Right Telescopic Bearing
Report Telescopic rail for railway and vehicle applications
White paper Rollon Linear Guides for the Train Industry
Whitepaper Anticorrosive Coatings Protect Train Components
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
Report How To Choose The Right Telescopic Bearing
Application Note Self-Aligning Linear Guides For Aircraft Seating
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
Application Note Showering Guests with Luxury
Application Note Retail Expansion Demands Unique Motion Control Solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Report Telescopic rail for railway and vehicle applications
Application Note Linear Bearing System Adds Critical Extra Space to Mobile Hospital Design
Report Linear Guide Alternatives
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Tech Talks Cleanroom-ready linear motion, engineered for precision
White paper Choosing linear motion components for medical equipment
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Report Linear movement in the pharmaceutical and medical industry: the seventh axis for clean rooms
Tech Talks Cleanroom-ready linear motion, engineered for precision
Case Study High-tech distributor taps Rollon for electronics machine
Case Study How Rollon actuators helped a Korean multinational corporation automate its battery cell manufacturing process
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
Case Study Automating a production line for the transport and machining of electrical wires
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges