• TUR
  • Download Area
  • myRollon
  • Aramak
  • Giriş
  • Hakkımızda
  • Ürünler
  • Sektörler
  • Haberler & Medya
  • İletişim
Rollon’a Sor
  • Hakkımızda
    • Hakkımızda
    • Markalarımız
    • The Timken Company
  • Ürünler
    • Linear Components
      • Lineer Kılavuzlar
      • Teleskopik kılavuzlar
      • Kavisli kılavuzlar
    • Actuators and Systems
      • Lineer Aktüatörler
      • Aktüatör Sistemleri
      • Robot Transfer Units
      • Dairesel Sistemler
    • Ball Screws
      • XP Xtrem Position
      • XL Xtrem Load
      • XT Xtrem Transport
    • Rotational Units
      • Çubuk uçları
      • Kaymalı rulmanlar
      • Rulmanlar
  • Sektörler
    • Malzeme taşıma
    • Sağlık Hizmetleri
    • Özel Araçlar
    • Bi̇na ve Mobi̇lya
    • Havacilik ve Uzay
    • Ambalajlama
    • Demir Yolu
    • Endüstriyel Makineler
  • Haberler & Medya
    • Kurumsal
    • Etkinliker
    • Yenilik
    • Medya
  • İletişim
    • İletişim
  • TUR
  • Download Area
  • myRollon
  • Aramak
  • Giriş
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
Linear rails for protective doors of machine tools

Webinar

Introducing a machining center into a production workflow is often the key to increasing the productivity and efficiency of the process.

However, these are costly solutions which represent a company’s technological capital. Hence the need for anyone purchasing a machine tool to have a product which can last for a long time and ensure maximum reliability.

The protective doors of a machining centre, for example, despite being an element that is apparently external to the machine, actually play a crucial role in the operation of the machine itself.

Indeed, they ensure both that the internal mechanisms are protected and, more importantly, that the external environment – where the operators work – is kept safe from the contaminants generated by machining processes, such as shavings, fine dust, and metal fragments.

That is why it is so important for them to continue to open and close smoothly and effectively over time. Any hitches in the operation of the machine’s doors would lead to a machine stoppage, with direct consequences on productivity.

What are the key features to consider when choosing the best linear motion solution?

In other words, what characteristics must a linear motion solution absolutely ensure to keep a machining centre effectively sealed? Which linear rail should a designer of machine tools choose to operate its doors?

There are many factors to take into consideration when selecting the right linear rail:

1. Managing misalignments to reduce the overall costs of the application and reduce installation times

The first and most important factor is the ability of the rail itself to manage imprecisions and misalignments in the surfaces it is mounted on (in terms of both parallelism and flatness).

In the case of the doors of a machining centre, we are dealing with a structure that is not particularly rigid or precise, as well as possibly having to manage significant misalignments, even of the order of a few millimetres.

This is where a self-aligning rail comes into its own as the ideal solution, as it is capable of preventing the need for costly modifications to the frame in order to increase its rigidity, or alternatively, equally costly mechanical work to the mounting surfaces. In addition, a linear rail which can manage misalignments simplifies installation, making it a great deal quicker.

2. Resisting corrosion to increase its working life

Another of the features to take into account is the linear rail’s resistance to the typically corrosive liquid refrigerants that the doors are designed to keep inside the machine.

The availability of a range of surface treatments which can be applied to the rail is a decisive variable when selecting a solution to install, as any solution must guarantee adequate resistance characteristics, such as those offered by passivated electro-galvanisation and nickel-plating treatments.

3. Reducing friction with larger rolling elements to ensure a fluid movement and maximum realibility

The door closing system for a machining centre is also subject to many “attacks” over the course of its lifespan.

The very same contaminants that represent a risk to the operators who work around the machine can actually be deposited on the raceways of the doors, causing them to jam over time.

Metal shavings, polymer dust, and even more minute particles result in increased friction, noise, and – in the long term – excessive wear and tear and blockage of the rail.

How can you solve the issue of the rail becoming blocked?

By using rails with roller bearings which, thanks to the large size of the rolling elements, have no trouble overcoming any obstacles present on the raceway, thus preventing jams, additional wear and tear, or compromising the efficiency of the door closing system.

COMPACT_RAIL_ROLLON

What’s more, integrating an optional combined raceway lubrication and cleaning system into the slider is unquestionably a highly valuable plus which allows for the system to stay running at peak efficiency for a long time.

Find out more about the advantages offered by Compact Rail, our range of rails with roller bearings, and compare them with recirculating ball bearing rails: take a look at the application examples and decide how to simplify your project, boost performance, and reduce costs.

Watch the webinar

Solutions by Industries

  • Herşey
  • Havacılık
  • İnşaat ve Mobilya
  • Endüstriyel Makineler
  • Tıp
  • Ambalajlama ve lojistik
  • Demiryolu
  • Özel Araçlar
Uygulama İlaç ve tıp endüstrisinde doğrusal hareket: temiz odalar için yedinci eksen
White paper Korozyon: ihtiyaçlarınız için doğru işlem
White paper Doğrusal sistemlerin yanlış hizalanması nasıl telafi edilir
SPEEDY RAIL, AKILLI VE "DAİMİ" LİNEER RAY
White paper YABANCI MADDE SORUNLARI İÇECEK ENDÜSTRİSİ OTOMASYONUMU ETKİLİYOR: NE YAPABİLİRİM?
Report Performans Sağlayan Teknoloji: Rollon’un Speedy Rail Lineer Kılavuzları
Report Yukarıdan sarkan yükleri teleskopik kılavuzlarla hareket ettirme: Rollon’unmeydan okuması
Uygulama SFC ve Business Class koltuk
Report X-Rail Li̇neer Raylara sahi̇p lüks Duşlar
Uygulama Sürgülü havuz kapağı
Uygulama Sürgülü pencere
Uygulama Dikey sürgülü ayak koruması
Uygulama Asansör kapısı açma/kapama sistemi
Uygulama Duş kapısı açma/kapama sistemi
Report Performans Sağlayan Teknoloji: Rollon’un Speedy Rail Lineer Kılavuzları
Report Tıbbi görüntüleme: güvenli ve doğru uygulamalar için Rollon rayları
Report 3B bi̇yoyazici i̇çi̇n Rollon Li̇neer Aktüatörler
Report Rollon portal si̇stemi̇ i̇le seçme ve yerleşti̇rme i̇şlemi̇: i̇şte neden kullanişli olduğu
White paper Linear rails with roller bearings: features and fields of application
Uygulama Makine alet açma kapısı
Uygulama İlaç ve tıp endüstrisinde doğrusal hareket: temiz odalar için yedinci eksen
Uygulama X-Ray Machine
Uygulama Tavana monte X-ray (röntgen) makinesi
Uygulama Optometri makinesi
Uygulama Engelli kişiler için tuvalet
Uygulama İLIŞKIN ÜRÜNLERIN SEÇIMI
White paper YABANCI MADDE SORUNLARI İÇECEK ENDÜSTRİSİ OTOMASYONUMU ETKİLİYOR: NE YAPABİLİRİM?
Report Intralojistik: Rollon rayları ile zamanında teslimatlar
White paper Linear rails with roller bearings: features and fields of application
Uygulama Teleskopik kavrama
Uygulama Mekik hareketi
Uygulama Kutu ambalaj
Report Demi̇ryollari sektöründe i̇ndüksi̇yonla sertleşti̇rmeni̇n sağladiği avantajlar
Uygulama Özel hareketler
Uygulama Koltuk ayarı, sürgülü masa
Uygulama Bakıp ekipmanı
Uygulama Yolcu kapıları ve basamaklar
Uygulama Platform perde kapılar
Uygulama Taşıyıcı genişletme
Uygulama Açma kapısı sistemi
Uygulama İç çekmeceler
Uygulama Dışa çekilebilen ekran
Uygulama Koltuk ayarı, kontrol paneli hareketi
Uygulama Koltuk ayarı, kızaklı çekmece

Rollon’a Sor

  • Hakkımızda
    • Hakkımızda
    • Markalarımız
    • The Timken Company
  • Ürünler
    • Linear Components
      • Lineer Kılavuzlar
      • Teleskopik kılavuzlar
      • Kavisli kılavuzlar
    • Actuators and Systems
      • Lineer Aktüatörler
      • Aktüatör Sistemleri
      • Robot Transfer Units
      • Dairesel Sistemler
  • Custom Menu
    • Ball Screws
      • XP Xtrem Position
      • XL Xtrem Load
      • XT Xtrem Transport
    • Rotational Units
      • Çubuk uçları
      • Kaymalı rulmanlar
      • Rulmanlar
  • Sektörler
    • Malzeme taşıma
    • Sağlık Hizmetleri
    • Özel Araçlar
    • Bi̇na ve Mobi̇lya
    • Havacilik ve Uzay
    • Ambalajlama
    • Demir Yolu
    • Endüstriyel Makineler
  • Haberler & Medya
    • Kurumsal
    • Etkinlikler
    • Yenilik
    • Medya
  • İletişim
    • İletişim
    • Bizi takip edin
      • LinkedIn
      • YouTube
Rollon
Nadella
Shuton Ipiranga
Durbal
Chiavette Unificate
Rosa Sistemi
© Rollon S.r.l. Via Trieste 26 20871 Vimercate (MB) C. Fiscale e P. Iva 05999150963 CAP. Sociale € 11.365.026,00 REA MB-1857623
  • Gizlilik Politikası
  • Cookies Policy
  • Genel Satış Koşulları
  • Kalite Politikası
  • Genel satın alma şartları ve koşulları
  • Davranış Kuralları
  • Krediler
  • Belgelendirmeler
TIMKEN

Ülkenizi seçin

Europe

cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sv-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Rollon’a Sor

Uzmanlarımız karşılaştığınız zorlukların üstesinden gelebilir