myRollon to cyfrowa platforma robocza firmy Rollon zaprojektowana w celu uproszczenia wyboru i konfiguracji rozwiązań ruchu liniowego i obrotowego.
Selection Tool
Selection Tool
Konfigurator
Konfigurator
Product Center
Product Center
Konto
Konto
?>
Najnowsze informacje
poniedziałek 12 maja 2025
Corporate & Events
Rollon świętuje 50 lat pionierskiej doskonałości w nowoczesnych rozwiązaniach do ruchu liniowego, kontynuując strategiczną globalną ekspansję
8 maja, 2025
Rollon świętuje 50 lat pionierskiej doskonałości w nowoczesnych rozwiązaniach do ruchu liniowego, kontynuując strategiczną globalną ekspansję
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
SPEEDY RAIL, INTELIGENTNA I „NIEKOŃCZĄCA SIĘ” SZYNA LINIOWA
19 września, 2023
SPEEDY RAIL, INTELIGENTNA I „NIEKOŃCZĄCA SIĘ” SZYNA LINIOWA
Read all
Chcesz się z nami skontaktować?
Kontakty
Kontakty
Twoje wyzwanie

Cartesian And Six-axis: Which System Is Best For Your Industrial Application?

Report

As more manufacturers automate their operations to improve productivity and competitiveness, different robotic systems have become available to perform a diversity of production tasks. Cartesian systems have been a workhorse in production facilities, while systems with articulated arms — such as the increasingly popular six-axis robot — have emerged to handle more nimble tasks. Depending on the application, there are clear rationale for using a Cartesian and clear rationale for using a six-axis system.

Advantages and Disadvantages

Here’s an overview of the advantages and disadvantages of each so you can select the right one based on your application needs:
Motion and manipulation

Designed for heavy-duty use, Cartesian systems typically work in the X, Y and Z axes of motion, and their reach is limited to the stroke of each axis. Six-axis articulated arms are well-suited for moving small items into position. They can manipulate parts through their many axes, and their pivoting points give them the ability to rotate a part.

Load capacity

Six-axis robots are supported by a pedestal. Although some six-axis systems can handle heavy loads, extending those loads beyond the pedestal can cause deflection issues, problems with moment of inertia and hinder accuracy. The X and Y axes of Cartesian systems are usually supported throughout their length with some kind of steel or aluminum frame, so they can support loads of 100 pounds or higher.

Speed and travel

Cartesian robots can travel both short and long distances, but they are easily scalable to whatever travel length is needed without major cost expenditures. The typical reach distance for six-axis robots is up to one and a half meters, but larger six-axis robots that can reach two meters and beyond are available. Cartesian robots can move loads at high speeds, but six-axis robots trade off some speed for better part manipulation.

Accuracy

Of the different types of Cartesian systems, ball-screw systems can achieve accuracies as tight as ±0.001 millimeter per axis. Six-axis systems can achieve ±0.050-millimeter accuracy.

Space

Because Cartesian systems have the benefit of being able to work from above as in an overhead gantry robot, they typically take up less floor space than six-axis systems.

 

New Advancements for Cartesian and Six-axis Systems

When it comes to industrial automation and robotics, Rollon’s Actuator System Line offers a variety of gantry and Cartesian systems as well as multi-axis systems. This product family can be found in numerous industrial applications from machinery servo systems to high precision assembly systems, packaging lines and high speed production lines supporting various load and motion requirements including specific speed, travel, orientation and positional accuracy. Product highlights include two particularly innovative systems:

  • Motion Box – a pre-configured Cartesian system that comes with every component necessary to deliver reliable motion while reducing associated set-up time, labor and expense.
  • Seventh Axis — a shuttle system that extends the operating area of a six-axis articulated robot so it can accomplish the same work as larger systems. That means more machines and processes can be serviced with one robot.

 

Both Robots Have Their Place


Manufacturers have to weigh the capabilities of Cartesian and six-axis systems with the motion, load handling, travel and accuracy requirements of the intended application in mind. Rollon Corporation’s Motion Box and Seventh Axis technologies can extend the benefits of these common robot types so plant managers can get the most functionality out of their implementations.

Solutions by Industries

  • Wszystkie
  • Budownictwo i wyposażenie wnętrz
  • Kolej
  • Maszyny przemysłowe
  • Medycyna
  • Opakowania i logistyka
  • Pojazdy specjalne
White paper Korozja: odpowiednia obróbka dla twoich potrzeb
White paper Jak skompensować niewspółosiowość systemów liniowych
SPEEDY RAIL, INTELIGENTNA I "NIEKOŃCZĄCA SIĘ" SZYNA LINIOWA
White paper PROBLEMY Z ZANIECZYSZCZENIAMI WPŁYWAJĄ NA AUTOMATYZACJĘ W MOJEJ FIRMIE DZIAŁAJĄCEJ W BRANŻY NAPOJÓW: CO MOGĘ ZROBIĆ?
Studium przypadku CZY COBOT MUSI ZAWSZE (I WYŁĄCZNIE) WSPÓŁPRACOWAĆ?
Studium przypadku ROZSZERZENIE OFERTY ZAUTOMATYZOWANYCH MAGAZYNÓW POPRZEZ INTEGRACJĘ ROZWIĄZAŃ AGV I SUWNIC LINIOWYCH
Report Prowadnice X-rail Firmy Rollon W Luksusowych Prysznicach
White paper Zalety hartowania indukcyjnego w branży kolejowej
Webinar Systemy prowadnic liniowych – najlepszy sposób na połączenie różnych zalet
Report Technologia w rozrywce: prowadnice liniowe Speedy Rail firmy Rollon
Jak Tips for Selecting an Industrial-Strength Telescoping Linear Motion Guide
Report Cartesian And Six-axis: Which System Is Best For Your Industrial Application?
Webinar Obrazowanie medyczne, prowadnice Rollon dla bezpiecznego i precyzyjnego badania
White paper PROBLEMY Z ZANIECZYSZCZENIAMI WPŁYWAJĄ NA AUTOMATYZACJĘ W MOJEJ FIRMIE DZIAŁAJĄCEJ W BRANŻY NAPOJÓW: CO MOGĘ ZROBIĆ?
Studium przypadku ROZSZERZENIE OFERTY ZAUTOMATYZOWANYCH MAGAZYNÓW POPRZEZ INTEGRACJĘ ROZWIĄZAŃ AGV I SUWNIC LINIOWYCH
Report Intralogistyka, dostawy na czas z prowadnicami Rollon
Webinar Ruch liniowy dla bezproblemowej paletyzacji
Report Pick-and-place z systemem suwnicowym firmy Rollon: jego zalety
Report Projektowanie Mobilnych jednostek medycznych przy użyciu Systemów prowadnic Liniowych
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Zapytaj Rollon

Nasi eksperci rozwiążą Twoje wyzwania