Wednesday 15 July 2026
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
Rollon and Dexis: bespoke cartesian automation for the packaging sector
15 July 2026
Rollon and Dexis: bespoke cartesian automation for the packaging sector
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
Educationals

Wall Mounted Robot Track Systems: Using a Seventh Axis Robot Track to Maximise Reach

In factories, the question is how to make robots them work smarter and in tighter spaces. That is where a wall mounted robot on a seventh axis robot track becomes interesting. Instead of placing the robot on the floor and letting it occupy valuable production area, the robot is suspended from an elevated robot track system, moving along the line like a gantry.

Wall Mounted Robots in Modern Industrial Automation

As production lines become more compact and more automated, every square metre of floor space counts. Machine tools, inspection cells, conveyors and operators often must share the same area.

A wall mounted robot travels on a track integrated into a rigid frame above the working area. The robot hangs from a carriage and moves laterally along the wall or an elevated beam, while still using its six rotational axes to perform tasks below. This is a wall-mounted Robot Transfer Unit configuration, where the linear axis is mounted horizontally on a frame and the robot is suspended from it to create an X-Y-Z wall of reach.

This arrangement is especially valuable in industries that want to keep the floor as clear as possible, for example when forklifts or AGVs move through the area, when regular washdown is required, or when operators need unobstructed access to machines. The wall-based robot track system lifts the seventh axis off the floor, while still providing the long stroke and positioning accuracy required in modern automation.

Motion and Layout Challenges That Favour Wall Mounted Robot Installations

There are some recurring situations where a wall-mounted seventh axis is particularly ideal. One is limited floor space, in factories where the layout is crowded with installed machines, structural columns and safety fences, fitting a floor rail between these elements can be difficult. Locating the seventh axis robot track on a wall or overhead frame can free the ground entirely, making it easier to reorganize workstations or introduce new equipment later.

Cleanliness and safety are also important factors to consider. When the robot track system is elevated, the line is easier to clean and to keep clear of debris. There are no rails to trip over and fewer places where dirt can accumulate.

Steel RTU-emea

Steel Robot Transfer Unit

The Seventh Axis Robot Track as an Elevated Robot Track System

In technical terms, a seventh axis robot track is a linear actuator that adds one more degree of freedom to a six-axis robot. Rollon’s Robot Transfer Units are long, railway-type axes that extend the robot’s working envelope by providing controlled linear motion along a straight path.

These Robot Transfer Units are designed as robust, modular systems that can be mounted on the floor, on the wall or even on the ceiling, depending on the application. The structure typically consists of an aluminium or steel body, precision linear guides, a rack-and-pinion or belt drive, and a carriage plate tailored to the robot’s base. In wall-mounted layouts, the track is fixed to a rigid frame or structural wall, and the robot is bolted to the moving carriage so that it travels horizontally above the work area.

How a Robot Track System Extends Reach, Safety and Flexibility

Adding a seventh axis turns a stationary six-axis robot into a mobile resource that can “walk” along the production line. The robot track system provides the long-stroke linear movement, while the robot’s joints manage the local positioning and orientation of the tool. Together, they create a large, flexible working envelope that would otherwise require multiple robots or very large gantries.

In a wall-mounted configuration, this extended reach becomes even more valuable. A single wall mounted robot can tend several machine tools in sequence, feed parts into different stations, or move between welding, inspection and packaging areas without ever obstructing the floor.

Why Rollon Robot Transfer Units Are Ideal for Wall Mounted Robot Applications

Rollon’s Robot Transfer Units have been developed specifically to extend robot reach in demanding industrial environments, and this experience carries over naturally to wall-mounted installations.

Rollon uses their know-how in heavy-duty actuators and precision linear guides to these robot tracks. The result is a robot track system with a high level of stiffness and repeatability, capable of supporting payloads from small cobots to large industrial robots, even when mounted high above the floor. Options such as covered belts, sealed bearings and rack-and-pinion drives help ensure reliable operation in dirty or harsh environments, which is common in welding, machining or material handling cells.

Choosing a wall-mounted seventh axis robot track is about balancing reach, layout and cleanliness. When floor space is at a premium, when processes are best accessed from above, and when production areas must stay clean, open and easy to navigate, elevating the Robot Transfer Unit can be a very practical solution.

FAQs

What is a wall mounted robot and how does it differ from a floor-mounted installation?

A wall mounted robot is fixed to an elevated structure or frame, usually with the seventh axis rail installed on a wall or overhead beam instead of on the floor.

How does a seventh axis robot track extend the working envelope of an industrial robot?

A seventh axis robot track adds linear motion to the robot’s six rotary axes, allowing the robot base to travel along a long stroke.

How can a robot track system help save floor space and improve safety in crowded production environments?

A robot track system mounted on a wall or overhead frame removes the rail from the floor, freeing up space for operators, pallets, AGVs and forklifts. With fewer obstacles and no floor rail to step over, traffic flow is cleaner, cleaning is easier and there is less risk of trips, collisions or damage to cables and mechanical components.

Which Rollon Robot Transfer Unit solutions can be used to build a seventh axis robot track for wall mounted robots?

Rollon’s Robot Transfer Units (RTU) can be configured for wall or overhead mounting to create a seventh axis robot track for wall mounted robots.

Related product line

Select the product line and start selecting

Steel RTU-emea

RTU (Steel)

1
Rack and pinion driven shuttle system for moving large robots and heavy loads. The highly engineered bases from steel allows for optimal high stiffness and load capacity.
RTU - Rack & PinionRTU - Sealed BeltRTU - Open Belt

RTU (Aluminium)

3
Belt and rack and pinion driven shuttle system for moving with high dynamics every model of robot, from the smallest cobot, to the largest robot.
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
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
White paper Motion designs for semiconductor manufacturing
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
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
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Report How to choose a rod end: A technical guide for design engineers
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
Report How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
Case Study Rollon helps AMP Automation to automate the palletizing process for a pet supplies company
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Case study: Rod ends for automatic packaging machines
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
Tech Talks Misalignment
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report Telescopic rail for railway and vehicle applications
White paper Rollon Linear Guides for the Train Industry
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper How linear motion powers restaurant automation
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Report Telescopic rail for railway and vehicle applications
Report Linear Guide Alternatives
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.

  • About Us
  • Products
  • Industries
  • News & Media
  • Contacts
  • myRollon
  • Rollon India Pvt. Ltd.
  • 39-42 , Electronic City, Phase-I, Hosur Road
  • Bangalore-560100, India
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges