Wednesday 15 July 2026
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
myRollon integrates roller guides in Configurator tool, releases new design for personal space and an optimized search bar
15 April 2026
myRollon integrates roller guides in Configurator tool, releases new design for personal space and an optimized search bar
Read all
Media
Rollon and Dexis: bespoke cartesian automation for the packaging sector
15 July 2026
Rollon and Dexis: bespoke cartesian automation for the packaging sector
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
Your Challenges

Key criteria for selecting linear motion solutions for high loads and speeds

Case Study

Inertial forces, mechanical stress, deflection, and cantilevered loads significantly affect performance, precision, and service life in robotics and automation applications. This whitepaper outlines the key criteria for selecting linear motion solutions to address these challenges, focusing on how to effectively manage the interplay between mass, acceleration, and overall system dynamics.

When specifying linear motion components for robotics and automation applications, the axes’ loads and speeds are key selection criteria. That’s especially true when axes involve heavy loads or high speeds – or both. After all, force = mass ´ acceleration, and machinery assemblies moving heavy payloads must output high forces to overcome their high inertias, especially when the quick accelerations and decelerations of high-speeds operations are involved.

Accommodating high loads

Robotic and automation installations must generate sufficient force to move their attached payloads. When payloads are especially heavy, there are other factors that must be addressed to ensure design safety, speed, and precision.

Elevated mechanical stress

Unless machine assemblies are designed for high loads, the effects of inertia can cause mechanical stress in their components and shorten their service life. High loads increase the forces on linear guides, rotary bearings, the teeth of racks in rack-pinion assemblies, and couplings.

More pronounced deflection

Unless actuator stiffness is prioritized, high loads can also cause axes to deflect. Even tiny deflections under dynamic loading can cause millimeter-scale positioning errors at machines’ end effectors, especially when axes are at their furthest reaches.

Gantry system for high loads and high-speed linear motion

Rollon® YZ PAR/PAS gantries include self-supporting extruded aluminum frames with high torsional rigidity and rack-pinion transmission for multi-axes in pick-and-place, industrial machine tending, and logistics. Some variations can transport payloads up to 2,000 kg over travels extending 12 m. Speeds up to 4 m/sec are possible.

Linear guides, actuators, gantries, and RTUs from Rollon come in aluminum and steel-frame variations (with subcomponents constructed of various precision-engineered materials) to resist torsion and deflection as well as wear and other challenges.

Magnified cantilevered-load effects

If the payload transported by an actuator, gantry, or RTU is at all cantilevered – as when a robot arm borne by an RTU reaches outward, for example – it demands more force than if the payload was perfectly rigid and centered on the carriage. With large loads especially, the offset distance from the gravity center to the axis’ center introduces significant pitching moments that force support structures, linear bearings, and drives to essentially resist rotation. That causes load redistributions within the bearings, which can make for higher friction, as well as structural deflection. The latter in turn coupes linear translation with a slight assembly rotation that can degrade repeatability and linearity over the stroke. In short, such moments can effectively create a dynamic penalty which can be quite significant if the payload has very high mass.

Suitable linear components and actuator solutions

Linear guides destined for dynamic axes often feature track-roller variations. These can provide payload capacity and stiffness along with high speed and acceleration. Rollon’s own prismatic rail and other roller-based guides – including Heavy Line  and V-Line – also withstand dirty or aggressive environments.

Consider just one example of a synchronous belt-driven product line built to handle high loads. Rollon® R-SMART and R-SMART-R linear actuators offer high load capacity with self-supporting extruded-aluminum structures. Widths from 120 to 280 mm bear and transport very heavy loads in automated equipment involving demanding work cycles and cantilever or gantry mounting. Multiple sliders can boost load capacity. The carriage is supported by twin linear guides that are profile rails pairs with recirculating bearing balls (R-SMART) or hardened prismatic rails that pair with track rollers (R-SMART-R). The R-SMART can run to 4 m/sec and 50 m/sec2 while the R-SMART-R can run to 8 m/sec and 20 m/sec2 and self-lubricating tanks or blocks with felts provide lubrication.

Linear actuator for high loads and high-speed operation

Rollon® R-SMART actuators can bear and transport very high load thanks to a rugged aluminum structure and substantial belt drive. The drive’s pulleys are large and have reinforced bearings for less stress on the motor and gearbox bearings (as slower motor rpm is possible with a larger pulley diameter). Shown here is the R-SMART 160; 230 and 280 versions extend the capabilities of these actuators.

Continue reading to discover how inertia impacts actuator sizing and system performance, the relationship between payload mass, acceleration, positioning accuracy and practical selection guidelines for robotics and automation applications.

Download the white paper
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
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
White paper Motion designs for semiconductor manufacturing
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
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
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Report How to choose a rod end: A technical guide for design engineers
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
Report How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
Case Study Rollon helps AMP Automation to automate the palletizing process for a pet supplies company
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Case study: Rod ends for automatic packaging machines
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
Tech Talks Misalignment
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report Telescopic rail for railway and vehicle applications
White paper Rollon Linear Guides for the Train Industry
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper How linear motion powers restaurant automation
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Report Telescopic rail for railway and vehicle applications
Report Linear Guide Alternatives
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.

  • About Us
  • Products
  • Industries
  • News & Media
  • Contacts
  • myRollon
  • Rollon India Pvt. Ltd.
  • 39-42 , Electronic City, Phase-I, Hosur Road
  • Bangalore-560100, India
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges