Wednesday 15 July 2026
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
Rollon and Dexis: bespoke cartesian automation for the packaging sector
15 July 2026
Rollon and Dexis: bespoke cartesian automation for the packaging sector
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
Your Challenges

How to choose a bearing based on load, speed and duty cycle

Report

Choosing the right bearing is a crucial decision to ensure performance, lifetime and reliability in mechanical systems. This article illustrates the main types of bearings, their structural and functional differences, and the technical criteria to consider when selecting the most suitable solution for your application.

Whenever a shaft needs to rotate relative to a support, a bearing comes into play. It is an essential component that allows turning by reducing friction while supporting the load.

There are different types of bearings:

  • Ball bearings
  • Roller bearings
  • Tapered roller bearings
  • Needle bearings

The difference between rollers and needles lies in their size: in needle bearings, the ratio between the needle’s length and diameter is greater than 3.

Another important difference concerns the presence of a cage. Bearings with cages can compensate for minor misalignments and operate well at high speeds; those without cages, on the other hand, are less tolerant of mounting errors but can withstand higher loads.

Nadella has been a pioneer in the development of needle bearings since 1930, the year it was founded. The name itself derives from the German term “Nadellager”, which means “needle bearing”.

Today, the Nadella range, an integral part of the Rollon portfolio, offers a wide variety of technical solutions:

  • Needle cages, which retain the needles both inward and outward and allow high-speed rotation.
  • Needle bushes, consisting of a thin, heat-treated outer ring, with or without a cage, capable of supporting high loads while occupying minimal radial space.
  • Needle bearings, with a hardened steel outer ring, available either with a cage or in a full-complement version.
  • Thrust bearings, in needle (AX) or roller (AR) versions, ideal for high axial loads in confined spaces.
  • Combined bearings, which integrate a needle cage and a thrust bearing into a single compact component, suitable for supporting both radial and axial loads.

Selecting the correct bearing depends on a combination of operating and environmental parameters. Let’s take a closer look at these.

Rotation speed and load

The first aspect to consider is rotation speed. In general, ball bearings are more suitable for high speeds, while needle bearings can withstand higher loads, but operate at lower speeds.

The presence of the cage also makes a difference:

  • with a cage, load capacity decreases but allowable speed increases;without a cage, there are more needles and therefore greater load capacity, but also more friction and lower speed.

Load direction

Another key parameter is the direction of the forces involved.

It is necessary to understand whether the load is radial (perpendicular to the shaft axis) or axial (parallel to the axis). For example, the AX bearings in the Nadella range are designed for axial loads only. RAX combined bearings, on the other hand, handle both radial and axial loads, offering a versatile solution in a single component.

AX needle bearings for axial and radial loads

AX Needle roller bearing

RAX needle bearings for axial and radial loads

RAX Combined bearing

Space requirements

When installation space is limited, a needle bearing is almost always the ideal choice. Its slim profile and high load capacity make it suitable for applications where space is at a premium.

Work cycle and type of movement

The lifetime and reliability of the bearing depend greatly on the operating cycle: how many rotations per minute, whether the load varies or remains constant, and the required service life, all of which influence correct bearing sizing.

Generally, needle bearings can operate with full or partial rotations but are not suitable for swivelling angles of only a few degrees. In these cases, the same needles would always be subjected to the motion, leading to localised and premature wear.

Materials

Most bearings are made of bearing steel, but the real difference lies in the material of the support on which they are mounted.

There are bearings with or without an inner or outer ring, and even cages with only needles. This configuration results in direct contact between the needle and the machine surfaces, which must feature adequate hardness and surface finish (e.g. grinding). If the correct material is not specified, there is a risk of reducing both the lifetime and load capacity of the bearing.

Lubrication and working temperature

Good lubrication is essential for the bearing’s lifetime. Greases or oils can be used, preferably with EP (Extreme Pressure) additives, which improve resistance to high contact pressures.

The choice of lubricant is also linked to the working temperature:

  • versions with rubber seals (generally ball bearings) retain grease better, but operate at temperatures up to approximately 120 °C.
  • all-metal bearings can reach higher temperatures, provided that specific high-temperature lubricants are used.

Finally, it should be noted that in needle bearings, contact is linear (rather than point contact as in ball bearings): this generates more friction and heat, making lubrication even more important.

Connect with Rollon Group

Choosing the right bearing is not just about finding a compatible component: it means optimising the entire system in terms of efficiency, durability and accuracy.

Thanks to Nadella’s experience and historical know-how, Rollon Group offers a robust technical portfolio capable of meeting many mechanical and environmental requirements.

If you would like to find out more about which solution is best suited to your application, contact us: our technical team is ready to assist you in choosing the most suitable bearing.

Connect with us

Related product line

Select a product to learn more

Needle Thrust Bearings

Nadella needle thrust bearings designed to support high axial loads while maintaining a small space requirement. This makes them particularly useful in applications where space is limited but high load carrying capacity and rigidity are required

Full Complement Needle Bearings

Nadella full complement needle bearings have a through hardened outer ring which results in high static and dynamic load capacities and an ability to withstand overloading, shocks and vibration. They are particularly suitable for operations involving oscillating motion but may also accept high speed conditions where good alignment is necessary

Combined Bearings

Nadella combined bearings designed to support simultaneously both radial and axial load. They comprise a needle thrust bearing and needle cage retained in a common outer ring. Their high radial and axial load capacities and small space requirement enable cost effective solutions to be achieved.
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
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
White paper Motion designs for semiconductor manufacturing
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
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
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Report How to choose a rod end: A technical guide for design engineers
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
Report How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
Case Study Rollon helps AMP Automation to automate the palletizing process for a pet supplies company
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Case study: Rod ends for automatic packaging machines
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
Tech Talks Misalignment
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report Telescopic rail for railway and vehicle applications
White paper Rollon Linear Guides for the Train Industry
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper How linear motion powers restaurant automation
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Report Telescopic rail for railway and vehicle applications
Report Linear Guide Alternatives
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.

  • About Us
  • Products
  • Industries
  • News & Media
  • Contacts
  • myRollon
  • Rollon India Pvt. Ltd.
  • 39-42 , Electronic City, Phase-I, Hosur Road
  • Bangalore-560100, India
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges