Wednesday 15 July 2026
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
Rollon and Dexis: bespoke cartesian automation for the packaging sector
15 July 2026
Rollon and Dexis: bespoke cartesian automation for the packaging sector
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
Educationals

Linear Guideways for Industrial Automation

Choosing the right linear guideways is one of the quickest ways to make a difference in industrial automation, not only in performance, but in how a machine can be built, aligned, and maintained over time. In many applications, the challenge is that structures aren’t perfectly machined, environments aren’t perfectly clean, and cycle rates are not gentle.

Roller-based solutions are often selected because they can operate quickly and quietly while managing mounting misalignments on the order of a few millimetres, in both parallelism and flatness, which supports design freedom in complex automation layouts.

Industrial Automation and the Role of Linear Motion Systems

linear motion systems in Industrial automation have to move something from A to B, precisely and repeatedly. That job however becomes harder because real machines are not assembled in laboratory conditions. Mounting surfaces may not be perfectly straight, frames can flex slightly, and dust or debris can be present even in regular production areas. In these situations, guideways that can tolerate small mounting imperfections help make the machine easier to build, easier to align, and more consistent from one build to the next.

That’s also why it makes sense to look at the full range of linear guides when designing automation equipment, different linear guide families are meant to match different loads, environments, and performance needs inside modern automation lines.

Motion Control Challenges in Modern Factory Automation Solutions

Even the best motion control systems can’t fix problems caused by friction, misalignment, or contamination in the mechanical axis. If a guideway starts to bind or get rough, the motion becomes less stable and repeatability can suffer. This is common in applications where dust, shavings, or residue are part of the process. Roller-bearing rails are often used here because they are designed to keep working reliably in tougher conditions, including environments with impurities that would otherwise accelerate wear.

Roller-Based Linear Guideways for Demanding Linear Motion Systems

Roller-based linear guideways become the right choice when the axis must stay stable under real-world conditions such as imperfect mounting surfaces, high-cycle operation, and demanding loads.If a linear guide can manage small misalignments without turning them into high friction or uneven wear, then the entire motion axis becomes more robust and easier to commission.

Within Rollon’s portfolio, looking at the broader range of linear slides helps define the most suitable architecture based on load, environment, and the performance targets of the application. Rollon’s linear guide rail systems have hardened raceways, rigidity, high load capacity, and self-alignment features that support operation even in dirty and demanding environments, exactly the conditions that often define modern industrial automation.

How Roller Linear Guideways Enhance Reliability in Motion Control Systems

Roller linear guideways help by keeping motion smoother under load and by reducing sensitivity to small alignment errors that can happen during assembly. In environments where dust and debris are present, roller-based designs can also be effective because they are commonly paired with protection and cleaning concepts that help keep raceways in better condition.

Why Compact Rail and Compact Rail Plus Are a Strong Fit for Industrial Automation Applications

When mounting quality and alignment are major variables, self-aligning families are often the most direct solution. Compact Rail is positioned specifically as a self-aligning linear rail system designed to solve misalignment issues and reduce machining time and application costs, an advantage when machines must be built quickly on structures that aren’t perfectly machined.

For applications that need the same self-aligning concept but with higher performance, Compact Rail Plus extends the capability with design features aimed at demanding duty cycles and tougher environments.This linear guide has increased load capacity and reliability in polluted environments supported by protective side seals and self-aligning scrapers that help clean the raceways.

There are also automation layouts where the guide must also act as a structural element, especially when space is tight and you want fewer supporting parts. In those cases, Speedy Rail is often a strong fit because it is designed as a lightweight, self-supporting linear rail with self-alignment properties and a maintenance-friendly approach for harsh or dirty environments. This linear guide self-alignment is enabled by the carriage concept and its performance characteristics intended for long-life operation without lubrication in demanding conditions.

Ultimately, roller-based linear guideways are the right choice in industrial automation when your priorities include tolerance to real-world mounting conditions, stability in contaminated environments, and long-term consistency for demanding linear motion systems. And when you need self-alignment and robustness without overcomplicating installation, families like Compact Rail, Compact Rail Plus, and Speedy Rail provide practical paths to reliable factory automation solutions.

Compact Rail TLC43 linear guide system showing lateral movement mechanism for locomotive seats

Rollon’s Compact Rail 

FAQs

What are roller-based linear guideways and how do they fit into modern linear motion systems?

They are linear guideways that use roller-bearing carriages to guide motion along a rail, in modern linear motion systems they’re used to keep movement stable and repeatable, especially under demanding loads and high-cycle operation.

When are roller rails preferable to other linear guide technologies in industrial automation?

They’re often preferable in industrial automation when the application is heavy-duty, runs continuously, or works in environments with dust and debris where robustness and long-term consistency matter most.

How do roller linear guideways help manage misalignment and imperfect mounting surfaces?

Many roller systems, especially self-aligning designs, are built to tolerate small mounting deviations, reducing binding risk and making installation easier on real machine frames.

Why are roller rails suitable for dirty, corrosive or noisy factory environments?

They can perform well in dirty conditions because roller elements can cope effectively with impurities and can be paired with sealing/cleaning features, and they’re available with corrosion-resistant materials or treatments, they’re also often chosen when smooth, quieter motion is a priority.

Related product line

Select the product line and start selecting

Linear guides with ball bearing roller

Compact Rail & Compact Rail Plus

2
Self-aligning linear guides with bearings and a C-profile made of cold-drawn carbon steel, with induction hardened and ground raceways.
Self-supporting linear guide - Speedy Rail

Speedy Rail

1
Self-supporting linear rail in extruded aluminum with steel rollers covered in plastic
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
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
White paper Motion designs for semiconductor manufacturing
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
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
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Report How to choose a rod end: A technical guide for design engineers
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
Report How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
Case Study Rollon helps AMP Automation to automate the palletizing process for a pet supplies company
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Case study: Rod ends for automatic packaging machines
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
Tech Talks Misalignment
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report Telescopic rail for railway and vehicle applications
White paper Rollon Linear Guides for the Train Industry
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper How linear motion powers restaurant automation
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Report Telescopic rail for railway and vehicle applications
Report Linear Guide Alternatives
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.

  • About Us
  • Products
  • Industries
  • News & Media
  • Contacts
  • myRollon
  • Rollon India Pvt. Ltd.
  • 39-42 , Electronic City, Phase-I, Hosur Road
  • Bangalore-560100, India
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges