Monday 27 July 2026
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
myRollon integrates roller guides in Configurator tool, releases new design for personal space and an optimized search bar
15 April 2026
myRollon integrates roller guides in Configurator tool, releases new design for personal space and an optimized search bar
Read all
Media
Selecting telescopic guides for train and railway-maintenance applications
27 July 2026
Selecting telescopic guides for train and railway-maintenance applications
Rollon and Dexis: bespoke cartesian automation for the packaging sector
15 July 2026
Rollon and Dexis: bespoke cartesian automation for the packaging sector
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
Your Challenges

Selecting telescopic guides for train and railway-maintenance applications

White paper

This whitepaper explores the key considerations involved in specifying telescopic guides for railway-maintenance systems and examines how different design approaches can address the unique challenges of rolling-stock applications.

Rail vehicles commonly house electrical and mechanical systems on heavy-duty trays supported by industrial telescopic guides. These systems can include battery banks for electric trains, HVAC units, converters, generators, compressors, and a wide range of auxiliary electrical and mechanical equipment.

Telescopic guides allow maintenance personnel to manually pull these systems out for inspection, replacement, recharging, cleaning, or repair while the train is stationary, and then safely return and secure them before the next journey.

However, railway applications rarely allow for a one-size-fits-all solution. Telescopic guides must support not only the weight of the equipment itself, but also the significant static and dynamic loads generated by train movement, braking, vibration, and shock. At the same time, they must enable a single operator to safely extend and retract very heavy equipment. This requires dimensional stability and resistance to binding, even when guides are fully extended and supporting cantilevered loads.

Environmental conditions add further complexity: depending on the vehicle and its operating routes, telescopic guides may be exposed to extreme temperatures, dust, sand, snow, and other challenging conditions.

These diverse operational requirements mean that selecting the right telescopic guide involves much more than matching a load rating to an application. This whitepaper explores the key considerations involved in specifying telescopic guides for railway-maintenance systems and examines how different design approaches can address the unique challenges of rolling-stock applications.

The role of telescopic solutions in rail maintenance systems

Telescopic guides for rail maintenance

Behind the many cutouts and access doors on a train are pieces of equipment on industrial-grade pull-out trays that ride on telescopic guides. © Rollon

Many maintenance-critical systems in modern rail vehicles are mounted on pull-out trays supported by telescopic guides, allowing safe and efficient access for inspection, servicing, and replacement.

One prominent example is the starting-battery system used in some electric trains. These battery banks provide the initial energy required to start and power the locomotive before it is connected to the catenary or electrical network. They are large, heavy components that require regular inspection, cleaning, and replacement throughout their service life.

Railway personnel may rely on forklifts to remove battery assemblies for maintenance. However, forklifts are not always readily available and often struggle to operate in the confined spaces typical of stations and maintenance depots. At the same time, maintenance windows are usually very limited. For example, metro trams may return to the depot after 1:30 a.m. and re-enter service as early as 4:00 a.m., leaving little time for servicing activities.

For these reasons, it has become common practice to mount battery boxes on heavy-duty telescopic guides, significantly improving maintenance efficiency. Operators can quickly extend the battery assembly from the car body, carry out the required work, and return it to its operating position without the need for additional lifting equipment. The same principle applies to HVAC systems installed beneath the train floor or within the car body structure.

Telescopic guides also support a variety of other railway applications. In some tram designs, they allow nose cones to slide laterally, providing maintenance personnel with access to earthing switches and other internal equipment. They are also used in storage compartments accessed through side doors or body panels.

Engineering considerations for railway maintenance systems

While applications differ in function, they share a common requirement: providing reliable, safe, and efficient access to equipment in environments where space is limited and downtime must be kept to a minimum. Achieving this requires careful attention to several design and operational factors.

Want to know more? Unlock the full whitepaper now to explore all the technical factors to consider when selecting telescopic guides.

Download the white paper

Related product line

Select a product to learn more

Partial extension telescopic railsPartial extension telescopic railsPartial extension telescopic railsPartial extension telescopic rails

Partial Extension

6
Compact telescopic slides composed of two elements for high rigidity and extensions from 50% to 70% of rail length.
Full extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic railsFull extension telescopic rails

Full Extension

29
Telescopic slides composed of three elements with different intermediate profile geometries for high rigidity and extensions of 100% of rail length.
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
White paper Selecting telescopic guides for train and railway-maintenance applications
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
White paper Motion designs for semiconductor manufacturing
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
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
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Report How to choose a rod end: A technical guide for design engineers
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
Report How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
Case Study Rollon helps AMP Automation to automate the palletizing process for a pet supplies company
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Case study: Rod ends for automatic packaging machines
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
Tech Talks Misalignment
White paper Selecting telescopic guides for train and railway-maintenance applications
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Report How to choose a rod end: A technical guide for design engineers
Report How To Choose The Right Telescopic Bearing
Report Telescopic rail for railway and vehicle applications
Case Study Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper How linear motion powers restaurant automation
Tech Talks Rollon’s Expanded Motion Solutions Portfolio
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Report Telescopic rail for railway and vehicle applications
Report Linear Guide Alternatives
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.

  • About Us
  • Products
  • Industries
  • News & Media
  • Contacts
  • myRollon
  • Rollon India Pvt. Ltd.
  • 39-42 , Electronic City, Phase-I, Hosur Road
  • Bangalore-560100, India
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges