Tuesday 5 August 2025
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
Educationals

Applications of Industrial Automation Systems

Industrial automation systems are enhancing production efficiency, not only by increasing speed but also by optimizing space and improving workflow flexibility. Among the solutions, circular systems stand out for their ability to create compact, customizable production lines by using linear and curved guides. 

 Why choose circular systems for industrial automation?

Circular systems are changing the way industrial automation systems operate by enabling complex and flexible layouts without limitations. Unlike traditional linear setups, circular systems combine curved and straight sections to form rectangular or oval circuits, ideal for continuous product movement within the different work stations. This configuration allows manufacturers to reduce machine footprints while maintaining high productivity. 

The ability to design compact production lines with independent yet adjacent workstations enhance ergonomics, simplifies operator access, and streamlines production workflows. This makes circular systems particularly effective for industries requiring efficient use of space without compromising operational efficiency. 

Features and benefits of curved guides

Curved guides are essential components of circular systems, offering smooth, precise movement across non-linear paths. These guides are designed to adapt to complex production layouts while ensuring durability and low maintenance. One of the key advantages is their customizable design, as they are available in various materials, sizes, and curvature radii to meet specific industrial automation system requirements.  

By incorporating circular systems and curved guides, production lines can achieve more compact layouts. This is particularly valuable in industries where floor space is limited, enabling businesses to increase productivity without expanding their facility footprint. 

Durability is another standout feature of these guides. Constructed from corrosion-resistant materials like stainless steel, they deliver reliable performance even in challenging environments. Additionally, the availability of optional self-lubrication systems further reduces maintenance demands while enhancing the overall lifespan of the guides. 

 Practical applications: packaging, medical, and more

The integration of circular systems within industrial automation systems offers significant advantages across multiple industries. In the packaging sector, circular systems streamline product flow between processing stations and enhancing efficiency. This allows manufacturers to maintain high output while offering consistency and accuracy throughout the packaging process. 

In the medical field, industrial automation systems supported by circular systems enable precise movement in diagnostic devices and filling lines.  

Rail transport also benefits from the use of curved guides.. These guides play a crucial role in train door mechanisms, allowing smooth operation along non-linear paths. This is especially important in space-constrained environments, where traditional linear systems would be impractical. 

By facilitating efficient, precise movement while optimizing space and reducing maintenance, circular systems have become an indispensable component of modern industrial automation systems, driving productivity and innovation across industries. 

 Solutions by Rollon and Nadella: Curviline and more 

Leading manufacturers like Rollon and Nadella offer advanced solutions for circular systems within industrial automation systems. Rollon’s Curviline series provides highly customizable curved guides with constant or variable radii, ideal for creating compact and flexible production layouts. 

Nadella products, such as the AXNR circular system, can be pre-tested at the factory to ensure fast, secure installation, minimizing startup times and enhancing overall plant efficiency. Advanced sensor integration further enables real-time system monitoring, facilitating predictive maintenance and reducing the risk of downtime. 

Circular systems represent a cutting-edge approach to industrial automation systems, empowering manufacturers to optimize production while maintaining flexibility and precision. From packaging to medical devices and railway applications, these solutions offer unmatched efficiency and adaptability. 

FAQs

What is an industrial automation system?

An industrial automation system is a technology-driven setup that uses machines, control systems, and software to automate manufacturing processes, improving efficiency and reducing human intervention.

What are examples of industrial automation?

Examples of industrial automation include robotic assembly lines, automated packaging systems, CNC machines, and conveyor systems used across industries like automotive, pharmaceuticals, and food production.

What is the best motion system for industrial automation?

The best motion system for industrial automation depends on the application, but circular systems with curved and linear guides offer superior flexibility, space optimization, and precision for complex production layouts

Related product line

Select the product line and start selecting

Curviline curved guide

Curviline

3
Curvilinear rails with radial ball bearing rollers (constant and variable radius)
Multi-Motion

Multi-Motion Line

1
Multi-Motion Line features induction-hardened raceways with circular-shaped rails combined with V-shaped bearing sliders. The rails can be used as an entire circumference, as single sectors or joined together to obtain oval or ring circuits.
AXNRQ

AXNR Circular System

1
AXNR circular system is composed of groups of standard elements: aluminium basement, guide rails and carriages, transmission by gearbox and toothed belt, lubrication units and carriage indexing for precise carriage location.
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
  • Food & Beverage
White paper Applying linear motion components in tertiary packaging machinery
Tech Talks Understanding Axial vs Radial Loads in Linear Guides
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
White paper The critical role of linear motion solutions in industrial machinery
How to How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
White paper Applications for industrial grade telescopic rails
Case Study Automating a production line for the transport and machining of electrical wires
Case Study CNC Solutions and Rollon: Advancing robotic automation for heavy-duty applications
How to How to choose a rod end: A technical guide for design engineers
White paper The critical role of linear motion solutions in industrial machinery
White paper Applications for industrial grade telescopic rails
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Report Monorail linear guide for high-load applications
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
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
MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges