Automating a production line for the transport and machining of electrical wires

Case Study

A high-tech company specialized in the design and production of electrical wires and connectors needed a customised curvilinear handling system to transport coils of electric wires through nine processing stations. The choice fell on Rollon® Nadella AXNRQ circular system in ring configuration.

With the continuous global rise of automated production systems, manufacturing companies face the challenge of integrating automation to maintain a competitive edge. Automation not only enhances efficiency but also improves flexibility, allowing plants to adapt quickly to new product designs and changing production demands. Moreover, automation reduces human error and ensures consistent product quality, making it a crucial investment for modern manufacturing facilities.

The challenge

A high-tech company specialized in the design and production of electrical wires and connectors needed an advanced automation solution to streamline its production process. Specifically, the company required a customized curvilinear handling system to transport coils of electric wires through nine machining stations while maintaining a cycle time of under two seconds between each stage.

Additionally, the system had to meet two other critical requirements: sufficient load capacity to handle coils of varying weights (8, 10, or 12 kg) and the ability to be installed on a 10-meter-long support structure already present inside the manufacturing plant.

With industrial automation playing an increasingly vital role in enhancing efficiency, flexibility, and product quality, finding a solution that optimized space, reduced manual intervention, and ensured high-speed operation was essential.

Automating Production Line Electrical Wires

AXNRQ Application example

The solution

After a thorough analysis of the application requirements, Rollon Nadella engineers proposed the AXNRQ circular system in ring configuration. This solution was selected due to its ability to meet the key operational demands of the project, offering:

  • High load capacity with robust guide rollers that support loads in all directions, helping ensure smooth and stable transportation of coils.
  • Optimized acceleration and speed, meeting the stringent stroke time requirement between machining stations.
  • Space-efficient design, allowing seamless integration onto the existing 10-meter-long support structure within the plant.

The system provided features a 10-meter-long circular track equipped with 24 carriages, ensuring continuous operation across all machining stations. Furthermore, to enhance reliability and minimize maintenance efforts, the solution includes an automatic lubrication system that helps ensure optimal performance over extended operational cycles.

Automating Production Line Electrical Wires

10-meter-long AXNRQ Circular System

The AXNRQ circular system delivers a fully integrated, ready-to-use circuit that allows manufacturers to achieve the desired performance while reducing footprint and engineering time. The core components of the system include:

  • Aluminum base for lightweight strength and easy installation.
  • Guide rails and carriages for precise and smooth movement.
  • Transmission system with gearbox and toothed belt for efficient motion control.
  • Lubrication units for extended durability and reduced maintenance.
  • Carriage indexing system to ensure accurate positioning at each processing station.
Automating Production Line Electrical Wires: Automatic Lubrication System

The automatic lubrication system

Automating Production Line Electrical Wires: the drive pulley directly mounted on the gearbox output shaft

The drive pulley directly mounted on the gearbox output shaft

The results

The implementation of the AXNRQ circular system has brought several benefits to the customer’s production process:

  • Improved motion control: the guide rollers contribute to stable and precise movement, helping to achieve accurate positioning of the coils.
  • Efficient use of space: The machined aluminum alloy base, directly connected to the gearbox, supports a compact and easy-to-install system.
  • Adaptability to specific needs: The modular and configurable design allows for a tailored approach to different production setups, potentially reducing installation time and engineering effort.

By adopting Rollon Nadella’s AXNRQ circular system, the company was able to implement an automation solution that aligns with its operational requirements, supporting efficiency and productivity improvements while optimizing the use of available space.

For more information on Rollon’s linear motion solutions and to connect with Rollon application engineers in your area or region, please get in touch with us.

Get in touch with us

Related product line

Select a product to learn more

AXNRQ

AXNR Circular System

1
AXNR circular system is composed of groups of standard elements: aluminium basement, guide rails and carriages, transmission by gearbox and toothed belt, lubrication units and carriage indexing for precise carriage location.
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
  • Food & Beverage
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
White paper Applying linear motion components in tertiary packaging machinery
Tech Talks Understanding Axial vs Radial Loads in Linear Guides
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
How to How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
White paper Applications for industrial grade telescopic rails
Case Study Automating a production line for the transport and machining of electrical wires
How to How to choose a rod end: A technical guide for design engineers
White paper The critical role of linear motion solutions in industrial machinery
White paper Applications for industrial grade telescopic rails
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Report Monorail linear guide for high-load applications
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
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
MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges