Monorail linear guide for high-load applications

Report

Rollon offers monorail linear guides for high-load applications such as machine tools as well as printing and textile machinery, food processing and packaging equipment, and industrial automation for other demanding industries. This Rosa Sistemi MG Rail line of products includes rails, carriages, and internal bearing rollers engineered and constructed to maximize rigidity and resolve normal and moment loads in all directions.

Permitted accelerations are to 50 m/sec2 and speeds are to 3 m/sec. The carriage is constructed of hardened alloy steel; the linear guide rail of hardened steel; and the rollers contained within the carriage of hardened bearing steel. Engineered with finite-element methods, the roller ways are constructed with geometries to optimize load bearing for specific preloads to maximize load capacity, performance, and accuracy.

In fact, the carriages have four circuits of recirculating rollers and are suitable for various arrangements on horizontal, vertical, and cross axes. These recirculating roller circuits impart high stiffness so essential to machine tool and similar applications.

Rosa Sistemi linear guides have stiffness values verified through testing that is repeated then averaged. Force is piezoelectrically measured between a hydraulic cylinder (applying force to the system) and the assembly plate to which the linear-guide carriage is fastened. With 0.1-µm resolution, an incremental optical linear encoder and strain gauges record deformation. The result is force versus stiffness charts plotting linear-guide behaviour under compression and tension. Shown here is a stiffness chart for MG55LL linear guides:

Four accuracy classes (Q0, Q1, Q2, and Q3) let engineers specify the linear guide with tolerances suitable for the application. In addition, two different preloads let engineers increase the system stiffness in exchange for a slight decrease in service life:

  • Preload class P2 is 0.08 C where C is the dynamic load rating. P2 is typically specified where an axis needs high stiffness and is subject to moderately high loads and intermittent vibration.
  • Preload class P3 is 0.13 C — typically specified where an axis needs maximum stiffness but is subject to impact loading, vibration, and high loads and moments.
Rosa Sistemi MG Monorail completes both the horizontal and vertical axes on this grinding machine.

Besides their high stiffness, Rosa Sistemi MG Rail also feature simplified lubrication of carriage roller ways through lubrication ports. In fact, to maximize design flexibility for machine builders, each carriage has four lubrication ports — one on each side and end. Lubrication input is controlled with check microvalves on both carriage sides to prevent backflow during linear-guide operation. No matter the linear-guide orientation, the system lets machine operators achieve optimal roller and way lubrication even while using modest quantities of oil or grease.

To complete this system, the heads of the carriage contain a gasket that seals the carriage and protects the ways. It is possible to apply additional wipers to reduce the risk of high contamination.

For more information, visit the MG Rail dedicated product page.

Discover more about MG Rail

Related product line

Select a product to learn more

MG Rail SL35MG Rail LL35

MG Rail

1
Profiled recirculating roller guides are precision mechanical components that ensure high load capacity and stiffness. These guides are composed of cylindrical rollers as rotating elements, ensuring high rigidity and stability.
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
  • Food & Beverage
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
White paper Applying linear motion components in tertiary packaging machinery
Tech Talks Understanding Axial vs Radial Loads in Linear Guides
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
How to How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
White paper Applications for industrial grade telescopic rails
Case Study Automating a production line for the transport and machining of electrical wires
How to How to choose a rod end: A technical guide for design engineers
White paper The critical role of linear motion solutions in industrial machinery
White paper Applications for industrial grade telescopic rails
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Report Monorail linear guide for high-load applications
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
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
MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges