• GBR
  • Download area
  • myRollon
  • Search
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
  • GBR
  • Download area
  • myRollon
  • Search
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
Wednesday 16 July 2025
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
How to choose a rod end: A technical guide for design engineers
26 June 2025
How to choose a rod end: A technical guide for design engineers
Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
25 June 2025
Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Read all
Need to contact us?
Contacts
Contacts
Educationals

Overhanging Loads: solutions for cantilever applications

The improper handling of overhanging loads in industrial applications can result in reduced system performance, excessive wear on components, and even failure.

That is why in this article we will discuss the key challenges associated with cantilever loads, the best practices to manage them, and the role of telescopic guides in addressing these challenges.

Definition of overhanging and cantilever loads

In mechanical systems, an overhanging load refers to any load that extends beyond the support structure, creating a bending moment. A cantilever load is a specific type of where one end is fixed, and the other end extends freely.

The farther the load extends beyond its support point, the greater the bending forces applied to the supporting structure. These forces, if unmanaged, can cause deflection, instability, and wear on components.

Managing overhanging loads

The main challenge with overhanging loads is managing the resulting bending moments. If not properly addressed, these forces can cause deformation, reduce precision, and increase wear on bearings and guide rails.  To make sure that the loads are managed safely there are some general overhanging load rules to keep in mind:

  • Distribute the Load Evenly: It is important to avoid concentrated loads on the overhanging section.
  • Limit the Length of the Overhang: The cantilever length when reduced lowers the bending moment.
  • Use Reinforcements: braces or additional supports should be incorporated where possible.

 Choose the right telescopic rails: It is important to choose the correct linear bearing for your overhanging load. The linear systems selected must be capable of handling both the vertical load and the resulting moments from the overhang. For engineers, understanding the overhanging load rules ensures that system components operate within their limits, enhancing system longevity and reducing maintenance costs.

Telescopic guides with ball bearingsManaging overhanging loads with telescopic guides

Telescopic guides allow for linear motion in systems with overhangs, providing the necessary support and stability. Rollon’s telescopic rails, for instance, are built to handle both dynamic and static loads while minimizing deflection. Their high load capacity prevents deformation and reduces wear, ensuring durability in systems with frequent cantilever forces.

Additionally, telescopic rails are offered in different materials such as aluminium, steel and stainless steel AISI 316L with hardened raceways, and different accessories in order to satisfy the most of the application requirements.

Telescopic rails are used, for example, to manage overhanging loads in automated storage systems used in warehouses. In warehouse automated storage systems, trays or drawers extend from racking units, creating cantilever loads that can cause sagging or misalignment if unsupported. This instability risks damaging the system and reducing operational efficiency.

By using telescopic slides, however, these systems manage overhanging loads more effectively. The guides provide smooth, controlled movement even when the stroke overcome the lenght of the rail, preventing deflection and maintaining alignment. This improves both safety and efficiency, ensuring reliable access to stored items without risk of jamming or failure.

FAQs

What industries most commonly face overhanging load challenges?

Industries like warehousing, bulding and furniture, and railway frequently deal with overhanging loads in systems such as automated storage, drawer extraction and battery box extraction.How do telescopic guides differ from linear guides for cantilever loads?
Telescopic guides can extend and retract to support cantilever loads over a longer range, while standard linear guides primarily offer fixed-length support and are less suited for handling bending moments.

Can telescopic guides be customized for specific applications?

Rollon’s telescopic guides can be tailored to meet unique load capacities, extension lengths, and environmental requirements across various industries.

Which printing method is better for small print runs?

Digital printing is better suited for small print runs due to its quick setup, cost-effectiveness, and ability to handle customization.

Related product line

Select the product line and start selecting

HGT Telescopic SlideDBN Telescopic SlideDMS Telescopic SlideDSS Telescopic SlideHVC Telescopic SlideNDC Telescopic SlideNTB Telescopic SlideTLAX Telescopic SlideTLN Telescopic SlideTLQ Telescopic SlideTLR Telescopic SlideTQAX Telescopic SlideTQN Telescopic Slidedbn43dedms63HGT_HGT-XHVCLTFLTH_LTH-SNDCNTBTLN-Ptlq43ptlr43pTQAXTQN-P

Full Extension

28
Telescopic slides with balls or ball bearings for full extension applications. Stroke of 100%.

Over Extension

6
Telescopic slides with balls for over extension applications. Stroke from 150% to 200%.
ASN Telescopic SlideHTT Telescopic SlideNTT Telescopic SlideNTT

Partial Extension

6
Telescopic slides with balls for partial extension applications. Stroke from 50% to 70%.
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
  • Food & Beverage
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
White paper The critical role of linear motion solutions in industrial machinery
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
Case Study Automating a production line for the transport and machining of electrical wires
Case Study CNC Solutions and Rollon: Advancing robotic automation for heavy-duty applications
How to How to choose a rod end: A technical guide for design engineers
White paper The critical role of linear motion solutions in industrial machinery
White paper Applications for industrial grade telescopic rails
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Report Monorail linear guide for high-load applications
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Podcast A Deep Dive Into The History Of Linear Bearings
Application Special Movements
Application Seat adjustment, sliding table
Application Battery box extraction
How to How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Case study: Rod ends for automatic packaging machines
Case Study Rollon helps AMP Automation to automate the palletizing process for a pet supplies company
Case Study Rod ends for material handling: challenges, advantages and solutions
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
How to How to choose a rod end: A technical guide for design engineers
Application SFC and Business Class seat
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
White paper White Paper: linear and curvilinear guides and systems for architectural and furnishing applications
Application Vertical sliding foot guard
Application Linear Motion Systems for Sliding Window Applications
Application Sliding pool cover
Application Wall aquarium slide out
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper White Paper: Preventing corrosion with stainless-steel and other motion components
Case Study Case study: Rod ends for agricultural machines
Application Display slide out
Application Interior drawers
Application Opening door system
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
MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sv-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges