Monday 8 September 2025
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
A lasting collaboration: Rollon supports Skyward and the Orion rocket at EuRoC 2025
8 September 2025
A lasting collaboration: Rollon supports Skyward and the Orion rocket at EuRoC 2025
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
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
4 September 2025
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
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
Educationals

Actuators for Heavy Duty Packaging Solutions

In sectors such as industrial packaging, selecting the appropriate actuator is a strategic investment. Whether the application involves heavy packaging, reinforced materials, or sensitive products requiring highly protective packaging, an actuator ensures reliability and continuity in the most demanding production environments.  

When dealing with heavy-duty packaging the demands placed on mechanical components, such as linear actuators, are significantly higher than in standard applications.  

What Are Actuators?

A linear actuator is a mechanical device that transforms various forms of energy, most commonly electrical, pneumatic, or hydraulic into straight-line motion. When used in packaging machinery, actuators control the movements of equipment involved in sorting, sealing, lifting, and transferring products along the line. Their role is to ensure that each movement is accurate, smooth, and repeatable, even under high loads or extended operating hours. 

In industries such as automated packaging facilities, actuators are often integrated into complete multi-axis systems. These configurations allow for synchronized control over several directions of motion, enabling faster cycle times and more complex operations.  

Multi-Axis

Key Requirements for Heavy Duty Packaging Applications

Heavy-duty packaging environments are characterized by a unique combination of physical stress and operational complexity especially when in automated packing. The loads tend to be substantial, whether due to the weight of the products themselves or the use of extra materials required for reinforced or highly protective packaging. This means that every actuator must deliver not only motion but also structural strength and longevity. 

In these packaging scenarios motion also must be precise, when involving fragile or high-value items, even slight deviations can result in damage or waste. The presence of vibrations, rapid acceleration and deceleration, or irregular environmental conditions can complicate performance requirements. Actuators operating in this space must, therefore, be built to handle continuous use without loss of accuracy or an increase in maintenance demands. 

Belt driven linear actuator - Plus System Robot

How to Select the Best Actuator for Heavy Duty Packaging

Choosing an actuator for heavy-duty packaging involves looking beyond speed or compatibility. It’s about understanding the specific nature of the application. For instance, if the system handles bulky products or operates at high throughput, the actuator needs to combine robust construction with reliable motion control.  

The material composition of the actuator, the type of guide system it uses, and its ability to maintain performance in contaminated or high-friction environments are also crucial considerations. Actuators featuring recirculating ball guides, for example, are particularly well-suited for packaging environments where wear and tear can quickly compromise efficiency.  

However, when a packaging system requires movement along multiple directions a multi-axis system becomes necessary. Unlike individual actuators, multi-axis systems are integrated assemblies that combine two or more actuators into a coordinated motion structure. These systems are ideal for complex automation setups and provide greater flexibility in layout and performance. Rollon offers modular, customizable multi-axis systems that are designed to handle the rigorous demands of heavy-duty packaging lines.  

By integrating Rollon’s linear solutions for packaging systems can achieve smoother operation, reduced energy consumption, and significantly extended service life. 

FAQs

What role do actuators play in industrial packaging solutions?

Actuators enable precise linear motion in packaging machinery, powering tasks such as lifting, sealing, sorting, and transferring products along the line. 

Why is proper specification crucial for heavy-duty packaging?

Proper specification ensures that actuators and motion systems can withstand high loads, harsh environments, and continuous operation without failure, preventing downtime and ensuring long-term performance in demanding packaging applications. 

Related product line

Select the product line and start selecting

E-SMARTR-SMARTR-SMART-RELMROBOTONE SeriesSABECOUNILINE AUNILINE CUNILINE EUNILINE EDMCHMCRCLSVERS-SMARTTLSZCH

Belt driven linear actuators

22
Rollon belt driven linear actuators combine performance, strength and versatility. Ideal for harsh environments and limited space, they offer high speed and precision, with steel re-enforced driving belts.
THTTTVTVSAMVAXNP-S

Ball screw driven linear actuators

6
The Rollon range of ball screw linear actuators are designed to provide extreme precision and repeatability in linear movements, making them ideal for industrial automation, packaging and robotics.
PARPASSARTLS

Rack and pinion driven linear actuators

4
Rack-and-pinion driven actuators in the Rollon range offer an excellent balance of payload, precision and durability, ideal for applications requiring long strokes linear motion.
2XYZ ESMART+RSMART+ SSMART2XYZ ESMART+RSMART+ZCH2XYZ E-SMART+ R-SMART+TH2XYZ PAR+PAR+PAS2XYZ PAR+PAS+PAS

XYZ Multi-Axis

5
Versatile multi-axis systems designed starting from your specific needs.
YZ PAS+PASYZ RSMART+ZCHYZ R-SMART+S-SMARTYZ RSMART+THYZ TH+THYZ SAR+SARYZ SAB+SAR

YZ Multi-Axis

9
Versatile multi-axis systems designed starting from your specific needs.
Steel-Multi-Axis

YZ Multi-Axis (Steel)

1
Rack and pinion driven steel multi axis systems for moving heavy loads.
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
  • Food & Beverage
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
White paper Applying linear motion components in tertiary packaging machinery
Tech Talks Understanding Axial vs Radial Loads in Linear Guides
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
How to How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
White paper Applications for industrial grade telescopic rails
How to How to choose a rod end: A technical guide for design engineers
White paper The critical role of linear motion solutions in industrial machinery
White paper Applications for industrial grade telescopic rails
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Report Monorail linear guide for high-load applications
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
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
MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges