Thursday 4 September 2025
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
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
4 September 2025
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
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
Educationals

How to optimize an automated production line

Optimizing an automated production line requires planning and a strategic selection of components. The goals of this optimization are enhancing efficiency, minimizing downtime, and overall improving the manufacturing process flow.

What is an automated production line?

An automated production line involves machinery that operates with little to no human intervention to complete repetitive tasks. These lines are commonly used in manufacturing industries that need to produce high volumes. Automated systems can include cartesian robots, robotic arms, conveyors, and sensors to carry out tasks such as assembling, packaging, and quality control.

By ensuring that components work seamlessly together, manufacturers can improve production line efficiency and maintain competitive advantages.

Streamlining the manufacturing process flow

The manufacturing process flow refers to the movement of materials and components through the various stages of production. Optimizing this is crucial as a smooth and efficient manufacturing process flow ensures that tasks are completed in a sequence without bottlenecks.

 To optimize these processes, it is essential to first identify the inefficiencies. To do so, it is often helpful to map the manufacturing process and review each stage where there are delays or resources are not being used. Implementing automation is also an important addition to optimise manufacturing processes flow. By integrating automation into repetitive tasks such as linear motion systems the overall production line efficiency can be improved.

Incorporating these strategies can transform a production line, making it more efficient, reliable, and capable of handling higher volumes without compromising quality.

How to select the right mechanical components for an automated production line

Selecting suitable components for an automated production line is essential to ensure long-term performance and reliability. Key factors to consider include:

  • Load capacity: to ensure components can handle the loads they will encounter.
  • Durability: components should be able to withstand high speeds and repetitive motions without frequent maintenance.
  • Precision and accuracy: linear motion systems must offer high positioning accuracy to avoid errors in the manufacturing process.

Choosing the right components can improve manufacturing process flow and production line efficiency, reducing downtime and maintenance costs.

Telescopic-RailsTelescopic rails used in production lines

Telescopic rails, such as those by Rollon, are integral components in many modern automated production lines. In the most advanced automation systems, such as those involving industrial machines or automated warehouses, telescopic rails are used for a variety of solutions, including cantilevered extractions of moving parts or enclosures, drawers, telescopic forks on AGVs, and often operate under critical conditions that include handling heavy loads, stressful cycles or high contamination environments. These guides facilitate smooth, linear movement, which is crucial for various applications that require both compact storage and extended reach. Their design allows machinery to operate with greater precision, stability, and reliability, making them invaluable across different industries.  One of the key advantages of Rollon’s telescopic rails is their availability with hardened and non hardened raceways, in a variety of materials, such as aluminum, steel, and AISI 316L stainless steel.  Additionally, Rollon offers customization options that enable manufacturers to tailor the guides to meet specific operational requirements, providing flexibility in how they are applied across different production lines.

FAQs

What is an automated production system?

An automated production system is a manufacturing setup where machinery and technology perform tasks with minimal human intervention, increasing efficiency and consistency in production processes.

How to automate an assembly line?

To automate an assembly line, manufacturers integrate technologies such as robotic arms, conveyor systems, sensors, and linear motion components to streamline repetitive tasks and improve production flow

What components are used in assembly line automation?

Key components used in assembly line automation include actuators, cartesian robots, linear and telescopic guides, conveyors, sensors, robotic arms, and control systems that work together to achieve precise, efficient, and reliable operations.

Related product line

Select the product line and start selecting

HGT Telescopic SlideDBN Telescopic SlideDMS Telescopic SlideDSS Telescopic SlideHVC Telescopic SlideNDC Telescopic SlideNTB Telescopic SlideTLAX Telescopic SlideTLN Telescopic SlideTLQ Telescopic SlideTLR Telescopic SlideTQAX Telescopic SlideTQN Telescopic Slidedbn43dedms63HGT_HGT-XHVCLTFLTH_LTH-SNDCNTBTLN-Ptlq43ptlr43pTQAXTQN-P

Full Extension

28
Telescopic slides with balls or ball bearings for full extension applications. Stroke of 100%.

Over Extension

6
Telescopic slides with balls for over extension applications. Stroke from 150% to 200%.
ASN Telescopic SlideHTT Telescopic SlideNTT Telescopic SlideNTT

Partial Extension

6
Telescopic slides with balls for partial extension applications. Stroke from 50% to 70%.
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
  • Food & Beverage
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
White paper Applying linear motion components in tertiary packaging machinery
Tech Talks Understanding Axial vs Radial Loads in Linear Guides
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
How to How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
White paper Applications for industrial grade telescopic rails
How to How to choose a rod end: A technical guide for design engineers
White paper The critical role of linear motion solutions in industrial machinery
White paper Applications for industrial grade telescopic rails
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Report Monorail linear guide for high-load applications
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
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
MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges