Thursday 4 September 2025
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
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
4 September 2025
Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
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
Educationals

Improving the Printing Machines in the Textile Industry with Compact Rail Plus

In the textile industry, in-motion printing is a groundbreaking approach that transforms how fabrics are decorated and personalized. However, to achieve consistent, high-quality results, this process depends on reliable linear systems capable of supporting smooth, accurate movements even in printing machinery operating at high speeds. 

When it comes to in-motion printing, the importance of reliable components is crucial. Linear systems must sustain stable, accurate travel across potentially long distances, all while enduring continuous operation and exposure to demanding environmental factors. 

Key Features of Compact Rail Plus for Innovative Textile Production

Rollon’s Compact Rail Plus stands out as one of the most versatile and powerful linear guiding solutions capable to meet the specific challenges of the textile industry. Engineered to handle heavier loads than many comparable products, it excels in environments where dust, fibers, and humidity could otherwise undermine equipment performance. By leveraging on a robust steel body and double-row roller bearings, Compact Rail Plus can withstand significant operational stress without compromising on smooth, quiet motion. 

A critical advantage of this system its in the ability to compensate misalignments. Structural misalignments often arise in large-scale production facilities where machinery may be installed on flooring or frames subject to slight irregularities. Compact Rail Plus tolerates misalignments of up to ±3.5 mm, allowing for easier setup and reducing the need for costly, time-consuming realignments. The result is a solution that not only simplifies the installation process but also promotes operational continuity. Maintenance requirements are minimized thanks to built-in protection against contaminants, ensuring the system remains functional despite the high volumes of dust and fiber particles common to textile environments. 

compact rail plus rollon

Why Compact Rail Plus is the Perfect Fit for Moving Print Systems in the Textile Industry

For printing machinery that handles substantial throughput, Compact Rail Plus is an ideal option due to its ability to deliver steady motion under intense operational pressures. In in-motion printing, a stable guide mechanism ensures that each drop of ink is accurately placed, maintaining alignment with the fabric’s speed and the system’s color registration. 

Another significant point is the system’s adaptability. Given that many textile producers look to upgrade existing machinery rather than invest in completely new lines, Compact Rail Plus’ compatibility with an array of setups is a crucial benefit. Instead of redesigning an entire production process, manufacturers can integrate these linear guides into their current framework, saving both time and financial resources. This adaptability encourages incremental improvements that keep pace with evolving market demands for personalized and fashion-forward fabrics. 

Where Compact Rail Plus is Used in Textile Industries

In the textile industry, linear systems aren’t restricted to in-motion printing alone. They are vital at multiple production stages, boosting precision, efficiency, and reliability. From highly accurate automated fabric cutting on large surfaces to the smooth handling of bobbins, these systems ensure uniformity, repeatability, and minimal alignment errors. 

They are also critical for finishing operations like coating and heat setting, delivering stable and controlled motion for uniform treatment. In applications such as embroidery     or automated cutting, the positioning accuracy they offer impacts the finished product’s quality. Overall, solutions like Compact Rail and Compact Rail Plus stand out for their versatility and performance in rigorous environments, including those with dust or fibers often found in the textile industry. 

FAQs

How does Compact Rail Plus support linear motion technology in textile printing machines?

Compact Rail Plus ensures precise, fluid motion at high speeds in printing machinery, improving print quality and reducing vibration. It handles heavy loads, tolerates misalignment, and offers minimal maintenance needs, fibers, and moisture commonly encountered in textile industry environments. 

What are the advantages of Compact Rail Plus for textile production?

In the textile industry , Compact Rail Plus provides robust, reliable operation under demanding conditions. Its compact design simplifies installation, compensates for structural misalignments, and extends service life. 

Related product line

Select the product line and start selecting

Compact linear guide

Compact Rail & Compact Rail Plus

2
Self-aligning linear guides with bearings and a C-profile made of cold-drawn carbon steel, with induction hardened and ground raceways.
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
  • Food & Beverage
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
White paper Applying linear motion components in tertiary packaging machinery
Tech Talks Understanding Axial vs Radial Loads in Linear Guides
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
How to How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
White paper Applications for industrial grade telescopic rails
How to How to choose a rod end: A technical guide for design engineers
White paper The critical role of linear motion solutions in industrial machinery
White paper Applications for industrial grade telescopic rails
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Report Monorail linear guide for high-load applications
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
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
MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges