Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive

Case Study

Railway maintenance requires precision, reliability, and above all, safety. In this article, you’ll discover how a custom-designed sliding seat mechanism featuring a linear motion system from Rollon helped technical crews improve lateral visibility aboard maintenance locomotives.

In the critical environment of rail maintenance, both safety and reliability are paramount. Often it can be the most unassuming components that deliver the biggest impact. This is the case with Rollon’s linear motion technology, which plays a critical role in enhancing visibility and safety aboard maintenance locomotives.

The challenge

Maintenance locomotives, unlike commercial trains, are purpose-built for technical crews responsible for on-track maintenance and inspection.

One of the practical challenges for optimising safety is ensuring engineers and mechanicians working onboard the maintenance locomotives have full lateral visibility to monitor the track and surrounding environment during operations.

In earlier configurations, seating within these technical locomotives was fixed, offering limited visual range to those onboard. With limited mobility, consistently overseeing work zones posed some logistical challenges especially on both sides of the locomotive.

Therefore, a leading European train operator contacted Rollon with a clear requirement: a lateral movement system that allowed engineers to reposition themselves swiftly and securely in response to dynamic maintenance conditions.

The solution

After thorough research and problem-solving, Rollon responded with its TLC43 and ULC43 Compact Rail, a robust linear guide system that provides smooth manual adjustment of seats. Mounted onto a basic metal sheet frame, this system enables precise lateral sliding of seats while withstanding the harsh conditions typical of maintenance environments, including dust, vibration and potential sudden impacts.

Rollon® Compact Rail

The TLC43 and ULC43 liner guide uses bearings rather than balls, making it particularly resilient in challenging settings. This choice also ensures a quieter and more fluid motion, allowing engineers to adjust position with ease without the need for power assistance. With a load rating of 150 kg under functional conditions and the capacity to endure 3G accelerations during emergency stops or abrupt movements, it is built to perform under pressure.

Crucially, Compact Rail also excels in its ability to compensate for misalignment. Unlike traditional systems that require precision-machined surfaces, Compact Rail can be mounted onto standard welded steel structures without the need for high-tolerance fabrication. This saves considerable manufacturing time and cost, offering a rugged and reliable solution that’s both efficient and affordable.

Compact Rail TLC43 linear guide system showing lateral movement mechanism for locomotive seats

Rollon® Compact Rail can compensate for misalignment.

A simple mechanism that improves safety and usability

The sliding seat functionality is more than a convenience – it directly supports safety protocols for a safer workplace. By allowing onboard engineers to slide across to windows on either side of the locomotive, they can maintain visual contact with colleagues working outside, monitor track conditions and respond quickly to hazards.

“This type of application really shows the strength of Compact Rail technology in harsh environments,” says Antoine Salomon, Key Account Manager at Rollon. “By using ball bearings, we can offer smooth, manual adjustment that doesn’t require power assistance or complex electronics. The ability to compensate for misalignment means our customers don’t need high-precision surfaces either, which is a huge benefit in industrial and rail applications where simplicity and durability are paramount.”

“The seat adjustment system in the maintenance locomotive is a perfect example of engineering minimalism at its finest. Motors and programming aren’t required – just robust, intelligent mechanical design that solves a very human problem. Rollon’s Compact Rail system proves that you don’t need complexity to achieve functionality. You just need the right combination of engineering expertise, durability, adaptability and understanding the customer’s needs.”

This application serves as a blueprint for how small changes in motion design can yield significant gains in usability, cost-effectiveness and safety. Rollon foresees wider application of the design principles in future builds or retrofits, with each implementation refined to match the customer’s specific operational needs.

For more information on Rollon’s linear motion solutions, please get in touch with us.

Get in touch with us

Related product line

Select a product to learn more

Compact linear guide

Compact Rail & Compact Rail Plus

2
Self-aligning linear guides with bearings and a C-profile made of cold-drawn carbon steel, with induction hardened and ground raceways.
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
  • Food & Beverage
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
White paper Applying linear motion components in tertiary packaging machinery
Tech Talks Understanding Axial vs Radial Loads in Linear Guides
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
How to How to choose a rod end: A technical guide for design engineers
White paper Linear motion in robotics and automation: Overview and trends
Case Study Midwest Engineered Systems (MWES) and Rollon: Advancing automation in heavy-duty material handling
White paper Applications for industrial grade telescopic rails
Case Study Automating a production line for the transport and machining of electrical wires
How to How to choose a rod end: A technical guide for design engineers
White paper The critical role of linear motion solutions in industrial machinery
White paper Applications for industrial grade telescopic rails
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Report Monorail linear guide for high-load applications
How to How to choose a rod end: A technical guide for design engineers
Case Study Case study: How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
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
MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
White paper CONTAMINANT ISSUES ARE AFFECTING MY BEVERAGE INDUSTRY AUTOMATION: WHAT CAN I DO?
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges