Tuesday 5 August 2025
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
Rollon’s Modular RTU: Built for Flexibility, Delivered in Weeks, Made in the USA
5 August 2025
Rollon’s Modular RTU: Built for Flexibility, Delivered in Weeks, Made in the USA
Applying Linear Motion Components in Tertiary Packaging Machinery
31 July 2025
Applying Linear Motion Components in Tertiary Packaging Machinery
Understanding Axial vs. Radial Loads in Linear Guides
28 July 2025
Understanding Axial vs. Radial Loads in Linear Guides
Read all
Need to contact us?
Contact form
Contact form
News and events

Streamlined Robotic Systems Help Manufacturers Combat Waste

Innovation | 19 April 2018

Cartesian robots are a particularly attractive automation option for manufacturers with pick-and-place type processes. Their highly precise motion boosts production efficiency, making them a natural choice for plant managers looking to cut waste. These robots let users concentrate their efforts on value-added processes that help the organization meet lean manufacturing goals.
 
 
Cartesian robots can help reduce waste that comes from:
  • Transport. Robots that perform pick-and-place operations can eliminate the need for multiple conveyors or personnel to move products from one production step to another. Products arrive at the next step when needed, and they don’t sit idle between steps.
  • Waiting. Cartesian robots provide motion within a defined framework and can be mounted in several configurations, so products move easily — even over long production runs and distances.
  • Motion. Heavier loads can be handled and transported while freeing up workers to perform more productive tasks and relieving operations managers from the worry of worker fatigue.
  • Defects. Reduced motion and handling by fatigued workers cuts down on dropped or defective products.
  • Overproduction. Manufacturers can build their products to order instead of building to sales or production targets, which can increase costly inventory.

Most Manufacturers Can Now Use Cartesian Robots
Cartesian robot systems now come pre-engineered and can include a three-axis robotic system using actuators, servo motors, controls and HMI together. Rollon’s easy-to-implement Motion Box system features load and speed charts to determine travel times for x, y and z axes with ease, ensuring the correct system for the application. It also accepts payloads up to 50 kg to outperform six-axis and SCARA systems while reducing ergonomic and health issues related to worker fatigue.

Since Motion Box is suitable for more than 80 percent of all Cartesian motion applications, most manufacturers now have the opportunity to use the most streamlined robotic technology available to maximize productivity and consolidate operations.

You may also like

Events IAS – Industrial Automation Shangai 2021
Corporate New Facilities, New Capabilities
Corporate Rollon bolsters its corporate social responsibility approach
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges