• Needle Bearings
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
Needle Bearings
Needle Bearings
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
Thursday 31 July 2025
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
Rollon Corp. Celebrates 50 Years and Future Growth with Opening of New Michigan Facility
13 June 2025
Rollon Corp. Celebrates 50 Years and Future Growth with Opening of New Michigan Facility
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
Applying Linear Motion Components in Tertiary Packaging Machinery
31 July 2025
Applying Linear Motion Components in Tertiary Packaging Machinery
Understanding Axial vs. Radial Loads in Linear Guides
28 July 2025
Understanding Axial vs. Radial Loads in Linear Guides
How to Choose a Rod End: A Technical Guide for Design Engineers
30 June 2025
How to Choose a Rod End: A Technical Guide for Design Engineers
Read all
Need to contact us?
Contact form
Contact form
Solutions by Industries

White Paper Explores Hardness Solutions In Linear Motion Rails

White paper

When it comes to linear motion rails, a high hardness value is critical. Unfortunately, some rail manufacturing processes don’t impart sufficient hardness to the rails. If hardness doesn’t extend to a sufficient depth, the component won’t be able to withstand heavy loads, resulting in time-consuming and costly downtime.

 

To gain maximum life for your linear guide, you’ll want to consider the hardening process, the material being hardened and how to finish the rail to optimize its performance. That way, quality manufacturers can make the best linear rail for your industrial application.

Consider induction hardening. To harden their rails, a manufacturer can use nitriding, a heat treating process that creates a case-hardened surface with thicknesses between 0.2 and 0.3 mm. When you consider the kinds of heavy loads that are applied to industrial raceways, rails that have thin nitrided surfaces will tend to crack under load.

Induction hardening, on the other hand, creates a zone around the raceway with depths up to 5 mm. Compared to gas furnace heating and other conventional heat treatments, the process offers several advantages, including fast heating rates, low energy consumption and cost savings. Rails will also operate under heavy loads with no damage to the raceways over the course of their lifetime.

Use high-quality steel. To achieve hardness levels that can stand up to the daily grind of industrial applications, high-quality linear motion rails need to be made from precise composition steel with a high carbon content. Induction hardening works by bringing out the natural properties of the metal, including its yield strength, malleability and toughness––which in turn increases the bearing’s strength and durability under variable loading conditions.

Rail Finish
Once a raceway undergoes induction hardening, its surface can be further machined to improve its anti-friction capabilities. Grinding also makes hardened raceways more precise. If two raceways aren’t parallel, then their running quality is affected.

By contrast, grinding cannot be performed on raceways that undergo nitriding and other similar processes. Because the resulting case-hardened surface is so thin, grinding would remove the hard coating entirely.

Download the White Paper

Related product line

Select a product to learn more

Compact Rail Linear GuideCompact Rail & Compact Rail PlusCompact Rail & Compact Rail Plus

Compact Rail & Compact Rail Plus

2
Self-aligning linear guides with bearings and a C-profile made of cold-drawn carbon steel, induction hardened and ground raceways. One of the biggest reasons that our customers prefer this model is the fact that it easily solves misalignment issues, due to its self-aligning system.

You may also like

White paper Anticorrosive Coatings Protect Train Components
Application Battery box extraction
Application Passengers doors and step
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
      • Needle Bearings
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges