Tuesday 5 August 2025
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
Rollon’s Modular RTU: Built for Flexibility, Delivered in Weeks, Made in the USA
5 August 2025
Rollon’s Modular RTU: Built for Flexibility, Delivered in Weeks, Made in the USA
Applying Linear Motion Components in Tertiary Packaging Machinery
31 July 2025
Applying Linear Motion Components in Tertiary Packaging Machinery
Understanding Axial vs. Radial Loads in Linear Guides
28 July 2025
Understanding Axial vs. Radial Loads in Linear Guides
Read all
Need to contact us?
Contact form
Contact form
Solutions by Industries

Differences Between Static & Dynamic Load Ratings

Blog Post

Static Load vs Dynamic Load

Data sheets and catalog pages for rolling element linear bearings or actuators provide two load capacity specifications — static load capacity and dynamic load capacity. These ratings can have a significant impact on your choice of linear bearing. It’s important to understand the differences between these two specifications so that you can properly evaluate and select an ideal bearing for your application. Note that some actuators may list a maximum force instead of a static capacity.

Understanding Static Load Capacity

Definition of Static Load Capacity

Static load capacity refers to the amount of a load the bearing can support in a given non-moving instance. This specification is typically designated as the symbol C0 and is measured in units of force, such as Newtons (N).

Importance of Static Load Capacity in Applications

The static load capacity is an important factor to consider when evaluating whether a system can withstand shock loads, repeated loading and unloading, and emergency stop conditions. If a bearing is subjected to a load that exceeds its static load capacity, the raceways may develop brinelling, resulting in noisy operation and premature failure. It is therefore crucial to choose a bearing with a static load capacity that is appropriate for your application’s needs.

How Static Load Capacity Was Defined

Historical Definition of Static Load Capacity

For many years, the basic static load capacity in a rolling element bearing was defined as the amount of load that would result in a permanent deformation of the rolling element equal to 0.0001 times its diameter.

Updated Standard

However, the standard has been updated to specify a load amount that can cause 480,000 pounds per square inch (psi) [3,310 megapascals (Mpa)] of Hertzian contact stress in the raceway. Regardless of how it is defined, be sure to check your static capacity safety factor using the following formula and guidelines:

  • Under normal load and operating conditions: f.s = 1-2
  • Under impact load or vibration operating conditions: f.s = 2-3
  • For best dynamic performance and service life, aim for a f.s >5.

Understanding Dynamic Load Capacity

Definition of Dynamic Load vs Static Load

Dynamic load capacity is not a stand-alone load rating, but rather a parameter used in an equation to calculate the theoretical service life of a bearing system. It is typically defined as C and specified in force units of N. At Rollon, our dynamic load capacity corresponds to a nominal service life of 100 kilometers of linear travel in accordance with DIN ISO 14728-1 in the United States and Europe. In some regions, the nominal service life is based on 50 kilometers.

Comparing Static and Dynamic Load Values

When comparing static and dynamic load values, consider the lowest value of the two as a starting point when assessing the bearing’s ability to carry the expected load. When specifying a bearing, it’s important to already know the weight of your static load and possibly your lifetime requirement, too. This information, along with the dynamic load rating, will help determine the lifetime capacity of the linear bearing system.

In most situations, multiple forces will act on your bearing. For example, if you anticipate a load that is 50 percent of the static load and also expect to see twisting, moment or other types of load, the lifetime calculation equation will incorporate these values as part of a single effective equivalent load value — P.eq, or just P.

theoretical service life

Use the Dynamic Load Rating To Calculate the Service Life

Rollon Linear Line and Service Life Formula

Rollon’s Linear Line of guides features a broad selection of product families like our Compact Rail, Compact Rail Plus with a double row of ball bearings, and Mono Rail profiled rail with recirculating ball bearings. When calculating the service life of our Linear Line, we use the following formula:

Expert Support for Accurate Calculations

We recommend talking to our experts to ensure accurate calculations. Our team will gather the relevant details about your application and ask the necessary questions to determine the appropriate service life calculation for your bearing. We will consider variables such as multiple bearings, environmental factors, and stroke distance, which can affect service life..

Factors Impacting Bearing Service Life

Environmental and Operational Considerations

Load factors are determined by taking into account all the loads that the linear bearing is expected to encounter in its application. When calculating service life, it’s essential to consider additional variables that can impact the bearing’s lifetime, such as the use of multiple bearings, environmental factors such as dirt or vibrations, and the stroke distance.

Shorter strokes may not allow the slider’s internal components to completely recirculate. This can prevent the reapplication of the lubricant on the bearing surfaces and therefore increase the likelihood of excessive friction and premature failure.

Rail Protection Options

For applications in corrosive environments, consider Rollon’s range of rail protection options before calculating service life. Our catalogs include look-up charts that enable you to factor in these variables when making your calculations. Moreover, if you expect your bearings to operate in a corrosive environment, consider Rollon’s many rail protection options before calculating service life

Gain Clarity to Select the Most Reliable Bearing

While static load capacity is a fundamental factor when sizing, buying and specifying any linear bearing, a proper understanding of dynamic load capacity is critical to ensuring it will perform reliably over its lifetime without incurring rail damage or failure.

At Rollon, we offer a wide range of quality bearings that can meet your linear motion requirements. Our engineering team can review your application details and help perform the dynamic load calculations so you can choose an ideal bearing that performs reliably over your target service life.

For more information about Rollon’s Linear Rails, visit our product pages.

Related product line

Select a product to learn more

Linear guides with ball bearing roller slider Compact RailCompact Rail & Compact Rail PlusCompact Rail & Compact Rail Plus

Compact Rail & Compact Rail Plus

2
Self-aligning linear guides with bearings and a C-profile made of cold-drawn carbon steel, induction hardened and ground raceways. One of the biggest reasons that our customers prefer this model is the fact that it easily solves misalignment issues, due to its self-aligning system.
Mono RailMono Rail

Mono Rail

1
Recirculating ball profiled linear rails with high load capacity and a high degree of precision. And with the recirculating ball motion system, this linear rail provides high stiffness.

You may also like

Application Loading/unloading of machined pieces: X-Y axes
Application Laser cutting machine
Application Z axis for machined pieces unloading
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges