• Needle Bearings
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
Needle Bearings
Needle Bearings
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
Monday 28 July 2025
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
Rollon Corp. Celebrates 50 Years and Future Growth with Opening of New Michigan Facility
13 June 2025
Rollon Corp. Celebrates 50 Years and Future Growth with Opening of New Michigan Facility
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
Understanding Axial vs. Radial Loads in Linear Guides
28 July 2025
Understanding Axial vs. Radial Loads in Linear Guides
How to Choose a Rod End: A Technical Guide for Design Engineers
30 June 2025
How to Choose a Rod End: A Technical Guide for Design Engineers
How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
24 June 2025
How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Read all
Need to contact us?
Contact form
Contact form
Solutions by Industries

Folded or Extruded Steel Rail: Choose The Right Rail For the Job

Report

When it comes to adding linear motion to a fixture, designers have to take a close look at the motion system’s rail construction. Linear guides and telescopic linear guides are typically made from two types of rail: folded rail — often called formed rail — and extruded rail. Some applications call for an extruded rail system while others are better suited for folded rail. As you determine which type of rail construction is right for your application, be sure to consider the following factors:

  • Your load handling requirements
  • Your extension requirements
  • Your expected cycling frequency
  • The operating environment
  • Deflections
  • Lifetime
  • Cost

With these factors in mind, it’s important to understand the construction and characteristics of each type of rail system:

  • Folded, or formed, steel rail can be desirable for low-load or low-cycle applications, or both. The rails get their shape from rolled steel, and they consist of two-to-four interior forms nested into an outer “C”-shaped form. Load capacity for a given form generally does not change with length, and if it does, it is a minimal increase. They also lack stiffness at load, resulting in higher deflection. Because folded rail is easier to manufacture and lacks the hardened raceways of extruded rail, it is less expensive. However, for applications with loads less than 200 pounds and less than eight cycles in an hour at or near rated capacity, folded rail can be very cost-effective.
  • Extruded rail is intended for high load capacities, reduced deflection, moderate-to-high cycling and a long service life. Because the steel is formed by extrusion, these rails offer a large cross section to give them a sturdier profile to handle heavy loads with less deflections. When telescoped, they can provide long extensions of 100 percent — even 150 percent — with the ball cage and sliders oriented back-to-back or top-to-bottom. Induction hardening brings out the tough material properties of steel, producing a thick zone around the raceway at the maximum point of stress beneath the rail’s surface. In fact, the resulting surface hardness exceeds the hardness of the base metal. That means it can offer a longer lifetime than folded rail under the same operating conditions. Induction hardened rails can achieve lifetimes ranging from thousands to hundreds of thousands of kilometers of travel.


Get the Most From Your Rail System

Rollon has a wide range of linear rail guides plus telescoping systems available with a choice of folded or extruded rail construction. Standard and custom products can meet various load capacities, extraction lengths and price points. And extruded systems can offer induction hardened raceways and resistance to shock and vibration. By understanding the benefits and drawbacks of each type of rail construction as they pertain to your design criteria, you’ll get a cost-effective system that satisfies your needs.

For more information about Rollon’s linear and telescopic rails, visit our catalogs page.

Visit Catalogs Page

You may also like

Report How To Choose The Right Telescopic Bearing
Report New Telescopic Rails For Aircraft Interiors Reduce Weight
Webinar Learn How to Design Smart at Our Compact Rail Webinar
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
      • Needle Bearings
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges