• USA
  • Download area
  • myRollon
  • Search
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
      • Needle Bearings
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
  • USA
  • Download area
  • myRollon
  • Search
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
Needle Bearings
Needle Bearings
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
Tuesday 8 July 2025
View all
Corporate & Events
Rollon Corp. Celebrates 50 Years and Future Growth with Opening of New Michigan Facility
13 June 2025
Rollon Corp. Celebrates 50 Years and Future Growth with Opening of New Michigan Facility
Rollon to exhibit RSN and AMTS 2025
11 June 2025
Rollon to exhibit RSN and AMTS 2025
Rollon to attend Automatica 2025
19 May 2025
Rollon to attend Automatica 2025
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
How to Choose a Rod End: A Technical Guide for Design Engineers
30 June 2025
How to Choose a Rod End: A Technical Guide for Design Engineers
How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
24 June 2025
How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Rollon Precision System Solution Helps JR Automation Deliver Increased Medical Device Assembly Speed
20 June 2025
Rollon Precision System Solution Helps JR Automation Deliver Increased Medical Device Assembly Speed
Read all
Need to contact us?
Contact form
Contact form
Solutions by Industries

Understanding Installation Differences

Report

For a case in point, consider what’s involved when switching from a ball-rail linear guide to Rollon’s Compact Rail.

The Compact Rail can replace any similarly sized ball-rail guide within the size, load and accuracy constraints described in the last post. Think of Compact Rail as a potential replacement for ball-rail guides.

We say “potential” because there is a difference in mounting pitch. While ball-rail guides typically have 50- or 100-mm mounting pitch, Rollon’s roller-style Compact Rails have an 80-mm pitch. With just a few minutes of CAD work, this difference is easily accounted for during the design stage. If a machine frame has already been prepped for a 50- or 100-mm pitch, the process of switching to Compact Rail would take more effort because custom made interface plates and brackets would be required.

There is an aspect to Compact Rail installation, however, that offsets any minor difficulties related to mounting pitch. Because it can self-align, Compact Rail does not require truly parallel mounting surfaces. In fact, it can tolerate large frame misalignments without losing an iota of performance or suffering from additional wear.

misalignment compact rail

How large? On rails 500 mm apart, for example, the Compact Rail system can tolerate rail height differences up to 20 mm. The system can also soak up misalignment in the horizontal axis–or when the rails toe in or toe out. The largest Compact Rail size can adjust to horizontal misalignments of nearly 4 mm over a 4080 rail length. The system can also accommodate angular misalignments up to +/- 2 degrees.

With ball-rail guides, the need to achieve parallelism during installation is one of the big cost drivers associated with the installation process. Mounting surfaces need to be ground or lapped carefully. And installers must go through the exacting–and expensive–process of shimming and bolting linear guides to the frame in a bid for near perfect parallelism.

In contrast to the exacting installation requirements for ball-rail guides, the Compact Rail typically adapts to the machine structure with a bit of screw tightening.This self-adjusting system does not require anything close to perfect mounting surfaces to work well. And that can be worth a lot more money than moving a few mounting holes.

Download the Catalog

Related product line

Select a product to learn more

Compact Rail Linear GuideCompact Rail & Compact Rail PlusCompact Rail & Compact Rail Plus

Compact Rail & Compact Rail Plus

2
Self-aligning linear guides with bearings and a C-profile made of cold-drawn carbon steel, induction hardened and ground raceways. One of the biggest reasons that our customers prefer this model is the fact that it easily solves misalignment issues, due to its self-aligning system.

You may also like

Tech Talks Misalignment
Webinar An Easy Way To Address Misalignment for High-Load Applications
White paper Avoiding Linear Bearing Failure Series
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
      • Needle Bearings
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sv-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges