• Needle Bearings
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
Needle Bearings
Needle Bearings
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
Thursday 17 July 2025
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
Rollon Corp. Celebrates 50 Years and Future Growth with Opening of New Michigan Facility
13 June 2025
Rollon Corp. Celebrates 50 Years and Future Growth with Opening of New Michigan Facility
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
How to Choose a Rod End: A Technical Guide for Design Engineers
30 June 2025
How to Choose a Rod End: A Technical Guide for Design Engineers
How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
24 June 2025
How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Rollon Precision System Solution Helps JR Automation Deliver Increased Medical Device Assembly Speed
20 June 2025
Rollon Precision System Solution Helps JR Automation Deliver Increased Medical Device Assembly Speed
Read all
Need to contact us?
Contact form
Contact form
Solutions by Industries

When to Choose Compact Rail versus Profiled Rail for Reliable Linear Motion

White paper

Profiled rail, also known as monorail or ball rail, is a tried and true linear guide system that incorporates small recirculating balls to satisfy tight positioning accuracy requirements. Often used in high-precision motion applications such as machine tools, these guides can achieve repeatability at the micron scale if correctly specified, installed and maintained. However, this level of precision can be both costly and unnecessary depending on the application.

 

Making sure the machine frame is flat enough, straight enough and parallel enough for profiled rails to be correctly mounted is no small task. In fact, the frame geometry itself can make it challenging to mount bearing rails parallel to one another in either the horizontal or vertical axis, or both. The result? Rolling elements and raceway surfaces are unevenly loaded, leading to pitting, noise issues and premature bearing failure. To avoid this, machine builders often spend significant time and money on surface preparation and machining to make sure bearing rails can go on perfectly straight and flat. But is all this preparation really necessary? Some high-end motion applications may call for exceptionally flat, straight and parallel mounting surfaces, but the truth is that most do not.

 

Another approach to handling misalignment and its associated problems is to use a self-aligning linear guide such as Rollon’s Compact Rail. This system is inherently forgiving of misalignment due to a unique rail geometry that compensates for alignment errors in one or two axes. In contrast to the demanding installation requirements for profiled rail, Compact Rail features large rolling elements, rail profiles that allow some play and an easy preload adjustment that enables equal loading of all elements. In other words, you get a more compliant guide than a profiled rail—and one that can align itself to less than perfect mounting surfaces.

When to Choose Compact Rail versus Profiled Rail for Reliable Linear Motion

It’s important to keep in mind that these two approaches—using high-precision profiled rail or a self-aligning system—can coexist in the same machine. For example, a machine tool spindle may demand a perfectly accurate linear motion system whereas a tool changer does not. Choosing the right linear guide for each axis based on individual requirements for precision and accuracy can save costs and achieve smooth, reliable linear motion at the same time.

 

A final point to keep in mind is contamination. With profiled rail, the small recirculating balls in the raceway have extremely limited clearance—meaning that even tiny pieces of dirt can interfere with motion. Bearings with larger diameter rollers such as those in Compact Rail can easily roll over much larger pieces of debris with no ill effects.

Download the Whitepaper

Related product line

Select a product to learn more

Compact Rail Linear GuideCompact Rail & Compact Rail PlusCompact Rail & Compact Rail Plus

Compact Rail & Compact Rail Plus

2
Self-aligning linear guides with bearings and a C-profile made of cold-drawn carbon steel, induction hardened and ground raceways. One of the biggest reasons that our customers prefer this model is the fact that it easily solves misalignment issues, due to its self-aligning system.

You may also like

Report Compact Rail Plus: linear motion freedom
Webinar An Easy Way To Address Misalignment for High-Load Applications
White paper Reducing Machine Design Costs: Eliminate Hidden Costs
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
      • Needle Bearings
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges