Key criteria for selecting linear motion solutions for high loads and speeds
11 June 2026
Key criteria for selecting linear motion solutions for high loads and speeds
Read all
Need to contact us?
Connect with Rollon
Connect with Rollon
Your Challenges

Ball screws vs. hydraulics: When to choose mechanical motion over fluid power

White paper

Across all industries, there is a global trend towards electrification — the design and use of motion systems based on electric motors rather than internal combustion, fluid power, or even manual means. The driving factor? An evolution is underway to make all industrial settings cleaner, quieter, and more efficient. Electric systems help machine builders satisfy all these objectives.

Leading the migration from fluid power to electric power are the machine-tool, aerospace, and off-highway industries.

For the special case of replacing hydraulic cylinders, electric-motor linear actuation can use rack-and-pinion sets, leadscrews and jackscrews, roller screws, and ball screws. However, ball screws are often the most efficient and viable of these options for replacing hydraulics.

This white paper details how ball screw-based actuation differs from that based on hydraulic cylinders — and where the two technologies compete. Also detailed are the sizes, geometries, and capabilities of large-format ball screws that offer an alternative to fluid power in challenging applications.

Ball screw actuation and variations

Ball screws — with typical maximum-output forces of 1 to 200 kN — are efficient and precise mechanical motion components that convert the rotary output of an electric motor into translational (linear) motion. The greatest benefit of these rotary-to-linear components is their extremely low-friction operation.

Ball screws include a threaded shaft that couples with the electric-motor output shaft to rotate with it. Fitted on this threaded shaft is a mating nut containing an array of load-bearing balls. The balls serve as the intermediate contacts between the nut’s ball-circuit surfaces and the raceways of the shaft threads — bearing any attached payload while rolling to allow the nut assembly to linearly travel along the shaft length.

In other words, as the shaft rotates, the balls travel along the shaft’s helical raceways to allow for output of linear motion. Once balls have run through the load-bearing course, with the help of a deflector on or within the nut assembly, they’re redirected and recirculated to the beginning of the circuit.

Discover our full range of ball screws and see how we can meet your application needs. Download the white paper now.

Download the white paper

Related product line

Select a product to learn more

IML / HDL / PKL

High dynamics and high load ball screws for injection molding machines, presses and other heavy duty applications operated by electric servo drive in extreme conditions.

Rolled

Rolled ball screws are an efficient solution for the linear drives requiring speed and load, but not the configuration and accuracy grade of a precision ball screw. The ball screws are manufactured by cold rolling process under the DIN69051 standard with accuracy classes IT5 and IT7.
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
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report Linear motion solutions for food processing
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges