Key criteria for selecting linear motion solutions for high loads and speeds
11 June 2026
Key criteria for selecting linear motion solutions for high loads and speeds
Read all
Need to contact us?
Connect with Rollon
Connect with Rollon
Your Challenges

Needle and cross roller guides: how they work and where they are used

Report

In this article, we explore the key differences between needle and cross roller guides and other linear guide technologies and analyse how to select the best option based on specific application requirements.

Needle roller and cross roller guides differ from recirculating ball or roller profile rail guides in a few fundamental ways.

The most significant difference is the type of bearing element used. Needle roller and cross roller guides rely on cylindrical rollers instead of balls distributed along the length of the guide. This design results in a much larger surface contact area compared to a recirculating ball rail, which directly affects load capacity, stiffness, and motion quality.

Cross roller guides use relatively large cylindrical rollers arranged in an alternating crossed configuration, with each roller positioned at a 90° angle to the adjacent one. This crossed arrangement creates extremely precise engagement between the rollers and the raceways, enabling high positioning accuracy and smooth linear motion.

Needle roller guides, by contrast, use tall, thin, needle-like rollers stacked in line with each other along the guide length. This geometry maximizes the contact area between the rollers and the raceways, allowing the guide to support much higher loads and achieve increased stiffness.

As a result, cross roller guides are typically selected for applications that require a combination of high load capacity and very high precision, while needle roller guides are preferred when maximum load capacity and stiffness are critical. In addition, unlike profile rail guides where the bearing elements recirculate inside the carriage block, the rollers in needle and cross roller guides are retained in position. This non-recirculating design contributes to very smooth and quiet movement characteristics.

Selecting the right guide for the right application

The Rollon Group portfolio – under the Rosa Sistemi brand – includes multiple needle roller and cross roller solutions designed to address different performance needs.

The GR rail, for example, is used in relatively high-load applications that demand very smooth, precise, and reliable linear motion with zero play. It is available with cages made from steel, polyamide, brass, or aluminium, allowing adaptation to various operating conditions and environments. Typical applications include high-precision machine tools, optical equipment, medical scanners, and laboratory equipment.

Another solution is the NG cross roller rail, which is designed to deliver especially high rigidity in a compact form factor. This makes it well suited for applications where installation space is limited but high performance is still required.

Needle and cross roller guides

GR guides

Needle and cross roller guides

NG guides

For even higher load ratings and rigidity, the RM RV needle roller guides are available. These guides are used in applications similar to those served by cross roller guides but are specifically selected when maximum stiffness and load capacity are required within the same footprint. Common examples include guides for EDM machines, grinding systems, welding equipment, and crimping or pressing machines. Various cage materials and roller configurations are available to meet specific application demands.

Needle and cross roller guides

RM RV needle roller guide

The portfolio also includes RM/RVA guides and M/V guides. Unlike the other solutions, these guides use full-contact antifriction material instead of bearing elements, offering an alternative approach for certain application requirements. They are typically used in low-speed applications that require maximum rigidity, such as substrate processing equipment, printing machines, and marble and glass processing machines.

Needle and cross roller guides

M/V and RM/RVA guides

To identify the most suitable guide for their specific application, engineers can use the selection tools available at my.rollon.com.

Selection Tool

Related product line

Select a product to learn more

Prismatic-Rail-RM-RVGR-NG

Cross Roller Rails

3
Precision linear motion components featuring four rows of cylindrical rollers offer high rigidity and accuracy for precise motion control. These components are designed for durable, low-friction operation, enhancing the performance of machinery in fields such as robotics, machine tools, semiconductor manufacturing, and medical equipment.
M/V

M/V and RM/RVA

2
Accurate and stable positioning due to raceways covered with anti-friction material promoting exceptional system rigidity while eliminating vibration.
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
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report Linear motion solutions for food processing
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges