Key criteria for selecting linear motion solutions for high loads and speeds
11 June 2026
Key criteria for selecting linear motion solutions for high loads and speeds
Read all
Need to contact us?
Connect with Rollon
Connect with Rollon
Your Challenges

How contamination affects linear guides and how to choose the right solution

Report

Contamination is one of the most critical factors influencing the performance and lifecycle of linear guides. In fact, not all guides react the same way when exposed to dirt, dust, liquids, or chemicals, which is why matching the guide type to the application environment is essential. In this article, we examine what contamination means in the context of linear motion systems, how it affects performance, and what design features help mitigate its impact.

In linear motion applications, contamination refers to any foreign material that increases friction along the guide’s bearing surfaces. This friction leads to uneven load distribution within the bearing. As contaminants accumulate, the risk of premature wear or even complete guide failure increases. For this reason, evaluating environmental exposure is a fundamental step when selecting a guide.

To simplify this assessment, contamination is typically classified into three main categories:

  • Large particle contamination
  • Fine particle contamination
  • Liquid contamination and chemical contamination

Each category affects guide performance differently, and not every guide design is equipped to withstand every environment.

Large particle contamination

Large contaminant particles include sawdust, machining chips, weld spatter, and similar debris. Fortunately, these contaminants can often be managed effectively, provided the guide includes the appropriate sealing or scraping elements.

For example, Compact Rail carriages are engineered with wipers that direct larger contaminants away from the raceway as the carriage moves, as well as side seals that prevent debris from entering the internal bearing contact surfaces.

Profile rail guides like MG Rail can also be outfitted with scrapers and seals capable of protecting the rollers inside the guide from large particles. When properly configured, these solutions typically maintain good performance even in environments where debris is abundant.

compact rail plus linear guide

Rollon® Compact Rail features wipers that clean the raceways.

Linear Motion Solution - MG Rail Linear Guide

Rollon Rosa Sistemi’s MG Rail.

Fine particle contamination

Fine contamination includes materials such as very fine sand, ceramic dust, and fiberglass particles. Because these particles can bypass many standard seals and scrapers, they pose a more significant challenge, especially for guides with open, recirculating ball bearings.

In such environments, fully sealed roller bearings offer superior resistance. The roller bearings used in Compact Rail and X-Rail systems, for example, can tolerate fine particles on the raceway.

By contrast, guides with exposed bearing cages should be avoided whenever fine particulate exposure is expected.

For telescopic applications operating in contaminated environments, Rollon’s full extension guides, such as TLN-P and TLAX, provide an effective alternative. In addition to sealed bearings, they include wipers that actively push contaminants out of the rail, making them highly suitable for harsh or particulate-dense applications.

Rollon® X-Rail features fully sealed bearings.

Rollon® TLAX full extension telescopic rail.

Liquid and chemical contamination

Environments involving saltwater, washdown procedures, or chemical exposure require a different approach. In these cases, material selection and surface treatment become key to ensuring durability.

Rollon offers multiple material and coating solutions tailored for these conditions, including:

  • Full stainless-steel components, ideal for many corrosive or hygienic environments.
  • Zinc-nickel or nickel chrome plating for outdoor or marine applications.
  • Nickel plating for applications involving washdown chemicals (common in medical and food processing settings).
  • Surface-hardened black nitrite finishing for high-wear environments requiring enhanced durability.

Choosing the right combination of materials and coatings helps protect the guide from corrosion, degradation, and premature wear caused by liquids or chemical exposure.

Selecting the right guide for your application

When contamination is a factor – whether from particles, liquids, or chemicals – the performance and lifespan of a linear guide depend heavily on selecting the proper configuration. Seal design, bearing type, and material selection all influence how well a guide will handle its environment.

If your application is likely to encounter any form of contamination, consulting a Rollon engineer can help ensure the linear guide is specified correctly from the start. Our engineering team can support you in evaluating environmental risks and determining the optimal guide solution for long-term reliability.

Get in touch with a Rollon engineer to select the best guide for your application.

Connect with us
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
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report Linear motion solutions for food processing
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges