Wednesday 15 July 2026
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
Rollon and Dexis: bespoke cartesian automation for the packaging sector
15 July 2026
Rollon and Dexis: bespoke cartesian automation for the packaging sector
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
Your Challenges

Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files

Case Study

Root canal files are among the most crucial components of modern dentistry. Their manufacture requires high-performance materials and extreme precision. This case study examines how VDW – an endodontic pioneer with more than 150 years of expertise – designs and produces these instruments using custom-built machinery supported by Rollon Nadella’s high-accuracy needle thrust bearings.

Most of us are familiar with the unmistakable sight and sound of instruments in a dentist’s office. While these tools often evoke varying degrees of apprehension, they are indispensable for modern dental hygiene and restorative care. What may appear to be simple, standardized instruments are in fact the result of complex engineering and manufacturing processes. Root canal files, for example, begin their life as NiTi wire blanks and undergo grinding, twisting, heat treatments, electropolishing, and surface coatings – procedures that transform raw metal into flexible, fracture‑resistant tools capable of navigating the tight geometry of root canals.

VDW has helped shape the evolution of root canal therapy for more than a century and a half. The history behind today’s VDW began in 1869, when C. W. Zipperer founded an endodontic company in Munich. More than a century later, in 1972, the Zipperer company joined forces with Antæos and Beutelrock to form Vereinigte Dentalwerke (VDW). This merger consolidated deep expertise in endodontics and gave rise to the VDW brand known today for delivering complete workflows for root canal therapy, from preparation through obturation.

Designing the machine behind the tool

To manufacture its root canal files, VDW designed a dedicated machine that embodies decades of specialized know‑how.

The process is both rapid and exceptionally precise. The machine takes in the metal blanks, grinds and machines them, performs optical control, applies a black coating to improve visibility and length marking accuracy, and outputs one finished file every three seconds.

Given the high forces involved in material removal and shaping, the machinery must guarantee extreme precision while maintaining compact dimensions and high load capacity. As Andreas Vogel, Manager Maintenance and Facility at VDW, explains: “Accuracy is pivotal. But any component within the machine also needs to be able to handle heavy loads and strong acceleration forces.”

Despite these significant mechanical challenges, the process must remain delicate enough not to damage or fracture the thin, flexible files.

The Rollon Nadella solution

To ensure the precise motion of the machining heads while meeting stringent requirements for load capacity, acceleration, and compactness, each VDW machine incorporates eight special needle bearings from Rollon Nadella, installed to support the movement of the grinding heads.

These bearings not only help ensure the necessary accuracy but also withstand the high acceleration forces generated by the production process. “The AX needle thrust bearing from the Rollon Nadella range was chosen for its high accuracy. The rolling elements of a thrust bearing are retained and guided in radial pockets within the cage. The cage itself is retained in relation to the plate by means of a steel ring. This assembly is easy to handle and install and provides high axial load capacity while occupying minimal space”, explains Stephan Schott, Industry Manager Medical at Rollon.

AX needle bearings for axial and radial loads

The Rollon® Nadella® AX needle thrust bearing.

Speed is also a crucial factor: the grinding phase in which the AX bearing is used lasts only one second, demanding a bearing solution that can withstand constant, rapid, repetitive motion without performance degradation.

A collaboration rooted in decades of trust

VDW’s collaboration with Nadella for this specific machine began in 2001, but the relationship predates that: earlier Nadella components were already used on predecessor machines built in 1986, one of which still remains in operation. This longevity demonstrates the consistent trust between the two companies.

“It’s been a very long-standing collaboration, for which we are satisfied,” says Ilker Karadeniz, Process Optimizer at VDW. “Such partnerships are essential not only for guaranteeing reliable production but also for supporting continuous improvement. Close collaboration enables rapid feedback loops, tailored engineering solutions, and confidence in long-term supply and performance”.

Today, VDW is testing a redesigned version of its manufacturing machine, a process expected to last one year. This testing phase underscores the importance of ongoing innovation, particularly in industries where micrometric precision and high reliability are non-negotiable. Continued collaboration ensures that as manufacturing processes evolve, the components that support them evolve as well.

If you would like to find out more about which solution is best suited to your application, contact us: our technical team is ready to assist you.

Connect with us

Related product line

Select a product to learn more

Needle Thrust Bearings

Nadella needle thrust bearings designed to support high axial loads while maintaining a small space requirement. This makes them particularly useful in applications where space is limited but high load carrying capacity and rigidity are required
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
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
White paper Motion designs for semiconductor manufacturing
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges