Key criteria for selecting linear motion solutions for high loads and speeds
11 June 2026
Key criteria for selecting linear motion solutions for high loads and speeds
Read all
Need to contact us?
Connect with Rollon
Connect with Rollon
Your Challenges

Linear motion solutions for food processing

Report

The food processing industry places stringent demands on linear motion systems: high-frequency cycles, strict hygiene standards, aggressive sanitisation processes and variable production layouts. This article explains how Rollon meets these challenges through solutions specifically designed for the food industry.

The food processing sector includes all operations related to the processing, handling, packaging, and movement of food along the entire production chain. From meat, fish, dairy, and baked goods processing facilities to packaging and palletising lines, these environments are characterised by strict hygiene requirements, high production rates, and intensive machinery usage.

Within this context, linear motion systems play a crucial role. They must deliver speed, operational continuity, and resistance to often harsh operating conditions. Key challenges include maintaining consistent performance over time, preventing food contamination, withstanding frequent and aggressive washdowns, and adapting to solutions that are often highly customised.

To address these requirements, Rollon offers a wide range of technologies developed specifically for the food processing sector, providing robust and reliable solutions that can be easily integrated into a variety of production layouts.

Speed and operational continuity

Food processing applications operate with continuous, high‑frequency cycles. Processes such as pick & place operations, rapid transfers between workstations, and synchronised movements during filling and packaging place severe dynamic demands on linear systems. These include high acceleration and deceleration rates, repeated directional changes, and high travel speeds. Under such conditions, the system’s ability to maintain consistent performance over time is essential to ensuring production continuity and quality.

Service continuity is a critical economic factor in food production plants. Production lines often run 24 hours a day with limited maintenance windows, meaning any unplanned downtime directly results in lost productivity. For this reason, component service life and predictable wear behaviour become design parameters of paramount importance.

 Rollon’s solutions

The Rollon portfolio includes actuators, linear guides, ball screws, and rod ends designed to meet demanding dynamic requirements. Their architectures are optimised to deliver fast, smooth, and precise linear motion, even under high‑frequency cycling conditions. These systems are engineered to maintain positioning repeatability over time, minimising mechanical performance drift even after a high number of operating cycles.

Particular attention is paid to the structural stiffness of the profiles, helping to reduce vibrations during acceleration and deceleration. This preserves the integrity of the handled products while reducing mechanical stress on components. A design philosophy focused on long service life minimises the need for downtime due to replacement or adjustment, contributing to maximised overall equipment effectiveness (OEE).

Prevention of contamination

In an industry governed by strict hygiene regulations, every component installed near the production line must be evaluated for its potential to cause contamination. This applies not only to parts in direct contact with foodstuffs but also to all components operating within the processing area that could release particles, lubricants, or residues into the surrounding environment.

Lubricants represent one of the primary risk factors. The migration of conventional mineral greases into the product or working environment can result in non‑compliance of the final product. At the same time, food residues that accumulate on mechanical components during processing can reduce accuracy and accelerate system deterioration.

Rollon’s solutions

Rollon supplies components lubricated with food‑grade grease that complies with FDA and European standards, eliminating at the source the risk of chemical contamination from motion systems. The Plus series of linear actuators, for example, uses recirculating ball bearings with an integrated “lifetime” grease reservoir that helps ensure continuous, controlled lubrication and reduces maintenance frequency.

For applications requiring complete separation between the system and the external environment, Rollon offers sealed or pressurised solutions such as the the ELM linear actuator. The closed structure of this axis protects both the working environment and the internal components from liquid infiltration and process residues, providing a dual level of protection suitable for the most critical applications. The system can also be pressurised up to 0.7-0.8 atmospheres for additional protection.

ELM linear Actuator

The Rollon® ELM belt-driven linear actuator.

Corrosion resistance

Sanitisation procedures in food processing plants are typically carried out daily and involve high‑pressure water, steam, and chemical detergents, which are sometimes strongly acidic or alkaline. The intensity and frequency of these cleaning cycles expose mechanical components to significant chemical and physical stress, potentially degrading surface treatments, damaging base materials, and compromising system functionality in the short to medium term.

Surface corrosion of profiles and slides can introduce unwanted mechanical play, alter positioning repeatability, and, in advanced cases, lead to premature component replacement.

Rollon’s solutions

Rollon offers an extensive portfolio of solutions designed to operate reliably in environments subject to aggressive cleaning procedures. The ELM and ROBOT actuators in their Corrosion Resistance versions, for example, feature guides and carriages made entirely from stainless steel. Structural steel parts can also be treated with specific surface finishes, such as nickel plating or zinc plating, selected according to the required level of protection.

The belt drive system is likewise optimised for these operating conditions. Internal stainless‑steel strands provide tensile strength and corrosion protection, supporting consistent mechanical performance over time. The combination of stainless‑steel materials, appropriate surface treatments, and effective sealing significantly extends component service life, reducing both replacement costs and downtime caused by component degradation.

Robot Actuators

The Rollon® ROBOT belt-driven linear actuator.

Customization

There are no truly standard applications in food processing. Each production line is the result of specific design decisions based on factors such as product type, production volume, plant layout, machine size constraints, and applicable regulatory requirements. As a result, linear motion systems must integrate into highly variable configurations, adapting both geometrically and dimensionally, as well as functionally and in terms of performance.

Rollon’s solutions

Rollon provides a high degree of customization for its linear systems, working in close co‑engineering collaboration with customers from the early stages of project development. This approach allows application‑specific requirements to be translated into optimised mechanical configurations that take dynamic performance, hygiene, chemical resistance, and dimensional integration into account simultaneously.

Thanks to the technical expertise developed through years of collaboration with leading food machinery manufacturers, Rollon can contribute effectively during the design phase by proposing the most appropriate solutions and anticipating critical issues from the outset. The result is a linear system that not only meets technical specifications but actively enhances the overall efficiency and reliability of the machine.

For more information, contact our team of Application Engineers.

Connect with us
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
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report Linear motion solutions for food processing
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges