Key criteria for selecting linear motion solutions for high loads and speeds
11 June 2026
Key criteria for selecting linear motion solutions for high loads and speeds
Read all
Need to contact us?
Connect with Rollon
Connect with Rollon
Your Challenges

Rollon and CAF: designing for reliability in rail interiors

Case Study

As part of a fleet refit programme, Spanish railcar manufacturer CAF faced recurring reliability issues with ageing toilet door mechanisms. Rollon was selected as the preferred linear motion partner to tackle this retrofit challenge.

Rail operators need to offer high levels of service reliability while managing ageing fleets, constrained maintenance windows and rising passenger expectations. While much attention is placed on traction systems, signalling and digitalisation, it is often the performance of smaller mechanical components that can have a significant impact on operations.

Interior systems, including doors, access panels and onboard facilities, are subject to constant use and challenging environmental conditions. When these components fail, the consequences can be immediate: service delays, increased maintenance interventions, and potential disruption to operations.

This is evident in areas such as onboard toilet modules, where space constraints, high usage and exposure to moisture and cleaning agents create a uniquely demanding application environment. Ensuring consistent performance in such conditions requires careful consideration of both design and component selection, particularly where movement systems are involved.

The challenge of constrained, high-use environments

As part of a fleet refit programme, leading Spanish railcar manufacturer CAF faced recurring reliability issues with ageing toilet door mechanisms on trains operated by Northern Ireland Railways.

In rail vehicle interiors, such as toilet door systems, components must operate reliably within compact, often irregular geometries, while maintaining performance within high frequency use.

Over time, traditional mechanisms can suffer from wear, which can cause jamming, ultimately leading to increased maintenance requirements and a higher likelihood of failure.

In operational terms, even a seemingly minor issue such as a faulty toilet door can escalate quickly. A door that becomes stuck or inoperable may render the facility unusable, negatively impacting passenger experience. In more severe cases, it can lead to disrupting timetables and increasing operational costs.

As a result, reliability is not simply a design preference, it is a critical operational requirement.

Limitations of conventional motion solutions

Historically, designers relied on a combination of straight linear guides and mechanical linkages to manage door movement within constrained spaces. However, these approaches often introduce compromises.

Straight guides can struggle to accommodate curved motion paths without additional components, increasing system complexity and installation time. Hinged or articulated systems, while capable of handling non-linear movement, may introduce points of wear and require frequent adjustment or maintenance.

In retrofit scenarios, these limitations become even more pronounced. Existing assemblies may not easily accommodate new components without significant modification, leading to increased downtime and higher installation costs.

For operators looking to extend the life of existing rolling stock while improving reliability, there is a clear need for solutions that can integrate seamlessly into existing designs while delivering improved performance.

A tailored approach to motion: curvilinear rail systems

To address these challenges, Rollon engineers proposed curved linear motion systems that combine flexibility with robust performance.

The choice fell on Curviline curved guide, designed specifically for applications where both linear and circular motion are required within a compact footprint. By allowing guides to be manufactured to precise angles, radii and lengths, the system enables designers to match the motion path exactly to the available space.

This ability to create custom geometries offers a significant advantage in retrofit projects, where existing layouts must be preserved. By specifying centreline radii, total length and hole pitch, Curviline rails can be integrated into existing assemblies with minimal modification, reducing installation time and disruption.

“Rail operators are looking beyond initial installation costs. They want solutions that deliver consistent performance over time, with minimal intervention” explains Lee Cheshire, Country Manager UK & Ireland at Rollon. “By combining hardened materials with optimised bearing design, we can significantly extend service intervals and reduce total cost of ownership.”

Curviline guide supporting rail interior reliability

Rollon® Curviline curved guide

Engineering for durability and long service life

Beyond geometric flexibility, durability is a key consideration in rail interior applications. Components must withstand continuous operation under demanding conditions.

Curviline systems address these demands through a robust design. They offer increased resistance to wear, while the ball-bearing sliders, lubricated for life, are designed to maintain preload across the entire length of the rail, even in complex curved configurations.

Material options further enhance performance. Depending on the application, rails can be supplied in galvanised, hardened or stainless steel, providing additional protection against corrosion where required.

This combination of features contributes to a longer service life and reduced maintenance requirements — key factors for operators seeking to minimise lifecycle costs.

Smooth, predictable operation

In addition to durability, consistent and smooth motion is essential for both functionality and passenger experience. Systems must operate quietly and reliably, without sticking, jolting or requiring excessive force.

Curviline’s low-friction design supports smooth travel along the entire motion path, while maintaining the required preload to prevent play or misalignment. This results in predictable performance over time, even in high-cycle applications.

The ability to mount rollers directly onto moving components in certain configurations can also reduce system thickness, offering further advantages in space-constrained designs.

Rail interior reliability enhanced with Curviline system

Rollon’s linear motion solutions such as Curviline offer a combination of flexibility, durability and ease of integration for rail interiors.

A successful outcome

“When we reached out to Lee and his team with a drawing of the part we needed to replace, it was quickly identified and a Curviline solution was proposed”, says Wallace Murphy, Performance Manager at CAF. “For context, the toilet system is fifteen years old. We received a rail set, including bearing assemblies, for twenty PMR toilet systems. Upon installation in the first toilet, there was a notable improvement in the quietness and smooth operation of the door. This solution will go a long way toward improving overall toilet system reliability, which is one of the most frequent customer complaints”.

 “The impact of component reliability extends far beyond individual systems. In a rail environment, failures can quickly cascade into broader operational issues. By contrast, solutions that deliver consistent, predictable performance help to maintain timetable integrity and reduce the burden on maintenance teams”, adds Cheshire. “As highlighted in the CAF project, the use of durable, customised motion systems can support more efficient operations and reduce overall costs. Across the rail sector there is a growing recognition that even relatively small components can have a major impact on overall performance. By focusing on reliability at every level, operators can avoid unnecessary disruption and keep services running smoothly.”

Supporting modern rail requirements

As rail operators continue to modernise fleets and extend asset life, the importance of component-level design is becoming increasingly apparent. Solutions must not only meet performance requirements but also support broader objectives, including:

  • Reduced maintenance interventions
  • Improved passenger experience
  • Faster and more efficient retrofits
  • Lower lifecycle costs

Curved guide systems such as Curviline align with these goals by offering a combination of flexibility, durability and ease of integration.

The CAF project demonstrates how combining custom geometry, durable materials and robust engineering can simplify integration, extend service life and, most importantly, support uninterrupted operation.

Interested in learning more about our solutions or starting a new project together?

Connect with us

Related product line

Select a product to learn more

Curviline curved guide

Curviline

3
Curvilinear rails with radial ball bearing rollers (constant and variable radius)
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
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report Linear motion solutions for food processing
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges