Key criteria for selecting linear motion solutions for high loads and speeds
11 June 2026
Key criteria for selecting linear motion solutions for high loads and speeds
Read all
Need to contact us?
Connect with Rollon
Connect with Rollon
Your Challenges

How Rollon helped a food company handle leavened doughs safely and effectively

Case Study

A leading Italian food machinery company contacted Rollon to develop a handling system for croissant and pizza dough along the production line. Specifically, the company needed a system to unload leavened doughs along a series of conveyor belts.

There were many challenges involved in the application. On the one hand, the level of efficiency of the entire process needed to be increased, reducing the cycle time compared to the previous self-built solution. On the other hand, the customer requested an increase in the system loading capacity while creating specific dynamics, as well as guaranteeing that the doughs were protected from contamination during handling. In fact, the solution had to be able to operate in an environment with a high risk of volatile dust contamination (typically flour and yeast), while ensuring that it would not contaminate the product. It also needed to withstand frequent cleaning with liquid detergents without damaging the surface or operations.

The Rollon solution

Given the processing, application and environmental requirements, Rollon chose to develop the application based on ELM linear actuators, placing them in a configuration involving two perpendicular conveyor belts. The dough is placed on the first and unloaded onto the second due to a retracting motion. The dough moves to the next station on the second conveyor belt.

The system acts via two different types of dynamics. The first working speed (0.6 m/s) is that of the dough moving from the first to the second conveyor belt. The second speed (1.3 m/s, more than double the first) runs backward (with a retracting motion). The sudden backward movement causes the dough to slip and land on the second conveyor belt. The acceleration handled by the system is about 3–4 m/s².

In the Rollon solution, two ELM 80 units from the Plus System series of actuators are coupled in parallel with double carriages and an interaxis distance ranging from 500 to 1000 mm, creating a useful stroke ranging from 1300 to 2000 mm. The load capacity of the system ranges from 150 to 300 kg and was sized for the processing requirements.

ELM Linear actuator

ELM Linear actuator

In addition, ELM actuators can be pressurized down to 0.7/0.8 atm, leading to a solution with an excellent seal for low air/energy dispersion. Finally, the lubrication used in the application involved vegetable greases specifically for the food industry and allowed by FDA standards.

The advantages of the system

The system designed by Rollon contained the key advantages required by the customer for the application.

On the one hand, all processing requirements were met: increased productivity, efficiency, load and dynamics. On the other hand, the application requirements were also met due to the construction of the ELM units. In fact, the chosen units easily handle the contamination risk involved in the application, making maintenance interventions unnecessary (the unit is isolated from external liquids and dust).

Due to the construction materials (anodized aluminum and stainless steel), the company can carry out the required cleaning without the risk of corrosion, even when using liquid detergents.

Finally, the company was able to rely on support from Rollon, both when analyzing the application requirements and when designing and installing the solution, capitalizing on Rollon’s experience in designing and implementing complete linear motion solutions and systems that can be customized to meet individual application needs.

For more information, contact our experts.

Contact us

Related product line

Select a product to learn more

E-SMARTR-SMARTR-SMART-RELMROBOTONE SeriesSABECOUNILINE AUNILINE CUNILINE EUNILINE EDMCHMCRCLSVER

Belt driven linear actuators

23
Rollon belt driven linear actuators combine performance, strength and versatility. Ideal for harsh environments and limited space, they offer high speed and precision, with steel re-enforced driving belts.
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
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Report Linear motion solutions for food processing
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges