Wednesday 15 July 2026
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
Rollon and Dexis: bespoke cartesian automation for the packaging sector
15 July 2026
Rollon and Dexis: bespoke cartesian automation for the packaging sector
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
Your Challenges

Preloading linear guides and actuators: when to do it and when to avoid it

Report

Preloading can be a make‑or‑break factor in many linear motion applications. This article explains the purpose of preloading linear guides and actuators and offers guidance on when preloading is beneficial, when it should be minimized or avoided, and how to determine the most suitable preload level for a given design.

A wide variety of linear motion components can be preloaded, including track‑roller bearings, profile‑rail guides, and linear drives such as ball screws and splines. In linear bearings and guides, preload is introduced by reducing or eliminating the clearances between the slider (also called a carriage), its rolling elements, and the linear rail.

The result is a more rigid assembly that operates without backlash and exhibits reduced deflection when supporting a payload. This is critical in precision motion‑control applications that rely on accurate, repeatable positioning.

Rollon MGB and profile‑rail linear guides offer a useful example of preloading in systems requiring high‑precision positioning of light to heavy payloads. Here, the sliding element is a block containing recirculating rows of balls.

These balls may be slightly oversized relative to the distance between the rail raceway surface and the ball track inside the slider. Slightly oversized balls can impart a preload of about 2% of the linear guide’s load capacity, while oversized balls can create higher preload of around 4%.

The Rollon MGB series comes in three preload classes: 

  • K0: Near‑zero preload for smooth motion.
  • K1: Light preload for improved rigidity, reduced deflection, and minimized vibration, balancing stiffness and fluid motion.
  • K2: Elevated preload for maximum rigidity under dynamic loads or vibrations, at the cost of increased friction and reduced life or acceleration capabilities.
MGB Linear guide

MGB linear guide.

How to select the most suitable preload

The optimal preload for a linear bearing or guide depends primarily on:

  • The number of rails used on an axis.
  • The achievable parallelism between parallel rails (where applicable).

For example, twin‑rail actuators, like Rollon Robot Plus or R-Smart, use pairs of carriages on parallel rails to provide four‑point support and minimize pitch, roll, and yaw. In such systems, increasing preload also increases alignment requirements. Insufficient alignment can otherwise introduce additional forces and moments that reduce lifespan.

Robot Actuators

Robot Plus linear actuator.

Rigidity and application dynamics are also key factors. Ball screws and linear motors often pair with moderately or heavily preloaded guides because the application demands that justify these drives typically also require high stiffness. A precision ball screw unit like the Rollon TT linear actuator benefits from a higher preload block to achieve high rigidity.

A higher preload can also prevent rolling‑element slippage during high accelerations, such as in systems driven by linear motors.

However, there are cases where excessive preload introduces drawbacks. In miniature designs or cost‑sensitive applications, preloading may shorten expected life or require larger, more expensive motors due to increased friction forces. Where preloading causes unacceptable heat generation, it should be reduced or eliminated.

In rare cases where preload may introduce static loading that is not fully counteracted by the axis payload, its effects on load capacity and system life should be carefully evaluated before making a final decision.

When preloading is essential

Light preload – typically 2% of a guide’s load capacity – is often required to maintain positioning accuracy in applications such as cutting, printing, assembling, packaging, medical imaging, and other true motion‑control roles involving light to moderate payloads. Light preload may also suffice in applications where payloads consistently move in one direction.

Moderate to heavy preload – 5%– is commonly required to prevent guide deflection in warehousing, machining, and other motion systems that transport larger loads. Higher preload is also crucial when minimizing deflection in cantilevered linear axes, such as those found on Cartesian robot end effectors.

Selecting the right linear system for your application

When preload is a factor, choosing the correct level from the start is essential for meeting performance, life, and cost requirements. Consulting a Rollon engineer can help ensure your linear system is properly specified for your application’s needs.

Connect with a Rollon engineer to explore the best guide solution for your system.

Connect with us
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
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
White paper Motion designs for semiconductor manufacturing
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges