Wednesday 15 July 2026
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
Rollon and Dexis: bespoke cartesian automation for the packaging sector
15 July 2026
Rollon and Dexis: bespoke cartesian automation for the packaging sector
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
Educationals

Linear Motion Components for Factory Automation and Motion Control Systems

In modern factory automation reliability is often won or lost in the details of how axes move, stop, and repeat. Whether you’re building a packaging line, a pick-and-place cell, or a modular station for automation in manufacturing, the performance of your linear motion components directly impacts uptime, accuracy, and total cost of ownership.

Factory Automation and the Role of Linear Motion Components

As machine automation becomes more modular and space-efficient, choosing the right linear motion components is part of good automation engineering, because the linear guide technology determines how sensitive the axis will be to mounting imperfections, contamination, and cycle intensity.

A key reason roller-based rails are used in factory automation is their ability to handle small misalignments in mounting surfaces. Instead of turning slight parallelism or flatness deviations into friction spikes and premature wear, roller-bearing rails are built to manage misalignments which can simplify machine design and reduce application costs tied to alignment and finishing operations.

Motion Control Challenges in Automation Engineering and Machine Automation

The toughest motion control problems rarely come from a single factor. They come from combinations such as high moment loads, short cycle times, dust, compact layouts and limited service access. In production, these challenges show up as vibration, noise, inconsistent positioning, and maintenance that arrives sooner than planned.

Roller-bearing rails address several of these pain points at the same time. They’re intended to run quickly and quietly while coping with mounting misalignment, which helps maintain repeatability when motion control systems are pushed hard by acceleration profiles and rapid stops. And because roller elements have a larger diameter than typical ball-based solutions, they can be more effective at dealing with impurities.

Roller-Based Linear Motion Components for Demanding Motion Control Systems

When you’re selecting guides for demanding motion control systems, if the machine frame can’t realistically be machined to tight tolerances, or if you want to avoid complex alignment steps during installation, roller-based rails can reduce the engineering burden without compromising robustness. Rollon’s approach combines linear guides with hardened raceways, industrial-grade profiles, and self-aligning concepts to support precision and durability across a wide range of applications, including dirty and demanding environments.

How Self-Aligning Linear Guides Support Automation in Manufacturing

Self-alignment is one of the most valuable features in real-world factory automation. It doesn’t just help the axis run smoother, but it can shorten commissioning time and reduce variability from one machine build to the next.

In roller-bearing rails, self-alignment is closely tied to the ability to manage mounting-surface misalignment. The result is often fewer corrective steps during installation and less reliance on perfectly machined structures which is an advantage when scaling machine automation across multiple lines or when building compact equipment where access for measurement tools is limited.

Compact Rail, a self-aligning linear guide family built around a C-profile concept that simplifies assembly and is commonly selected when misalignment is a real constraint in the project. Compact Rail is a solution that helps address misalignment issues thanks to its self-aligning system and hardened raceways.

Why Rollon Roller Rails Are a Ideal for Robotics in Packaging and Other Factory Automation Solutions

In robotics in packaging, linear motion often is used in end-of-line positioning, carton handling, infeed/outfeed management, and guided doors or guarding elements that must operate reliably at high frequency. These applications benefit from rails that tolerate imperfect mounting, remain stable under load changes, and keep moving even when the environment isn’t clean.

Roller-bearing rails are frequently chosen in packaging machinery because they combine misalignment management with strong behavior in dirty environments, dust, shavings, and processing residues are explicitly called out as conditions where roller-bearing rails can be especially effective.

For applications that need a cost-effective self-aligning concept in a compact format, X-Rail is another relevant option within the Rollon linear guides. The idea is that the combination of rail geometries to create an easy self-aligning parallel-rail system, with additional availability in corrosion-resistant versions such as stainless steel and surface treatments designed for harsher environments.

FAQs

How do roller-based linear motion components support modern factory automation?

They provide robust, repeatable motion under demanding loads and high-cycle operation, and they’re designed to tolerate real-world mounting conditions, which helps keep motion control systems stable and reduces downtime.

How do self-aligning linear guides help automation engineering teams deal with misalignment and flexible structures?

Self-aligning designs can compensate for mounting-surface deviations so frames that are welded or not perfectly machined are easier to assemble and commission without time-consuming alignment work.

Why are roller linear rails suitable for harsh, dirty or corrosive automation in manufacturing environments?

Roller rails can perform well in dirty conditions because the roller elements can be more effective at handling impurities, and they’re available with materials/treatments suited to humid or corrosive environments.

Related product line

Select the product line and start selecting

Compact linear guide

Compact Rail & Compact Rail Plus

2
Self-aligning linear guides with bearings and a C-profile made of cold-drawn carbon steel, with induction hardened and ground raceways.
ASN Telescopic SlideHTT Telescopic SlideNTT Telescopic SlideNTT

Partial Extension

6
Telescopic slides with balls for partial extension applications. Stroke from 50% to 70%.
HGT Telescopic SlideDBN Telescopic SlideDMS Telescopic SlideDSS Telescopic SlideHVC Telescopic SlideHGT-MG telescopic rail with redesigned ball cage and synchronization magnetsNDC Telescopic SlideNTB Telescopic SlideTLAX Telescopic SlideTLN Telescopic SlideTLQ Telescopic SlideTLR Telescopic SlideTQAX Telescopic SlideTQN Telescopic Slidedbn43dedms63HGT_HGT-XHVCLTFLTH_LTH-SNDCNTBTLN-Ptlq43ptlr43pTQAXTQN-P

Full Extension

29
Telescopic slides with balls or ball bearings for full extension applications. Stroke of 100%.

Over Extension

7
Telescopic slides with balls for over extension applications. Stroke from 150% to 200%.
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
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
White paper Motion designs for semiconductor manufacturing
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study Rollon and CAF: designing for reliability in rail interiors
Report Needle and cross roller guides: how they work and where they are used
Case Study A special rod end with linkage for the architectural structure of Princess Grace Hospital Centre: the Rollon Chiavette Unificate solution for Pontiggia Group
White paper Preventing corrosion with stainless-steel and other motion components
White paper Linear and curvilinear guides and systems for architectural and furnishing applications
White paper Corrosion: the right treatment for your needs
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
White paper Preventing corrosion with stainless-steel and other motion components
Report MiniRoller Rail and ELM: Rollon’s answers to the Meat processing industry
Case Study How Rollon helped a food company handle leavened doughs safely and effectively
Case Study Rollon collaborates with Siemens Healthineers on modern medical technology and pediatric patient experience
White paper Solving precision challenges: A Design Engineer’s guide
Report How contamination affects linear guides and how to choose the right solution
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Choosing linear motion components for medical equipment
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rollon Nadella and VDW: A long-standing collaboration for the precise manufacturing of root canal files
Report How contamination affects linear guides and how to choose the right solution
White paper Ball screws vs. hydraulics: When to choose mechanical motion over fluid power
White paper The critical role of linear motion solutions in industrial machinery
White paper Differences between ball screws for heavy equipment, automation, and machine tools
White paper Preventing corrosion with stainless-steel and other motion components
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
Case Study Turn-Key Solutions and Rollon: Engineering a robotic solution for an automated storage system
Case Study Rod ends for material handling: challenges, advantages and solutions
Case Study Expanding the automated warehouse offering by integrating AGVs and linear gantry solutions
Case Study Rollon and Dexis: bespoke cartesian automation for the packaging sector
Case Study How Rollon Durbal rod ends solved durability issues in GIC’s high-force VFFS packaging systems
White paper Applying linear motion components in tertiary packaging machinery
Case Study Rod ends for automatic packaging machines
Case Study Rollon and CAF: designing for reliability in rail interiors
Case Study How Rollon telescopic guides are redefining Business Class seating in rail
Case Study How Rollon’s Compact Rail enhanced visibility on maintenance locomotive
Report How contamination affects linear guides and how to choose the right solution
Case Study Enabling mobility through engineering: A custom linear motion solution for a Paralympic athlete's vehicle
White paper Preventing corrosion with stainless-steel and other motion components
Case Study Rod ends for agricultural machines
White paper Corrosion: the right treatment for your needs
White paper Key criteria for selecting linear motion solutions for high loads and speeds
Case Study HR Wallingford improves its wave-making systems with Rollon’s Compact Rail Plus
White paper How linear motion powers restaurant automation
Case Study Rollon supplies gantry system and RTU for Sangsin ENG’s brake pad production machines
Case Study Rollon precision system solution helps JR Automation deliver increased medical device assembly speed
White paper Linear motion in robotics and automation: Overview and trends
Report Linear motion solutions for AGVs and AMRs in vertical farming and greenhouses
Report Rollon linear solutions for vertical farming

Ask Rollon

Rollon - Motion Technology for All Types of Automation

For over 50 years Rollon has specialized in the production and development of linear motion systems, adopted worldwide in all those sectors where product performance, efficiency and reliability are essential. With the acquisition by The Timken Company of Nadella, Chiavette Unificate, Durbal, Shuton-Ipiranga, and Rosa Sistemi, Rollon is now able to offer its customers an even more comprehensive product range – from linear components, actuators and systems to ball screws and rotational units.
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges