• Needle Bearings
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
Needle Bearings
Needle Bearings
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
Tuesday 5 August 2025
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
Rollon’s Modular RTU: Built for Flexibility, Delivered in Weeks, Made in the USA
5 August 2025
Rollon’s Modular RTU: Built for Flexibility, Delivered in Weeks, Made in the USA
Applying Linear Motion Components in Tertiary Packaging Machinery
31 July 2025
Applying Linear Motion Components in Tertiary Packaging Machinery
Understanding Axial vs. Radial Loads in Linear Guides
28 July 2025
Understanding Axial vs. Radial Loads in Linear Guides
Read all
Need to contact us?
Contact form
Contact form
Solutions by Industries

Automating the electric wire production process

Case Study

A high-tech company specialized in the design and production of electrical wires and connectors needed a customized curvilinear handling system to transport coils of electric wires through nine processing stations. The choice fell on Rollon® Nadella AXNRQ circular system in ring configuration.

With the continuous global rise of automated production systems, manufacturing companies face the challenge of integrating automation to maintain a competitive edge.

For operations focused on industrial automation wire, automation boosts both efficiency and flexibility, making it easier to keep pace with evolving product designs and fluctuating production needs.

Automation also helps cut down on human error and delivers more consistent product quality, which makes it a smart investment for today’s manufacturing operations.

The challenge of the electric wire production process

A high-tech company specialized in the design and production of electrical wires and connectors needed an advanced automation solution to streamline its production process. Specifically, the company required a customized curvilinear handling system to transport coils of electric wires through nine machining stations while maintaining a cycle time of under two seconds between each stage.

Additionally, the system needed to support the demands of electrical wire manufacture, including sufficient load capacity for coils of varying weights (8, 10, or 12 kg) and compatibility with a 10-meter-long support structure already in place at the plant.

With industrial automation playing an increasingly vital role in enhancing efficiency, flexibility, and product quality, finding a solution that optimized space, reduced manual intervention, and ensured high-speed operation was essential.

AXNRQ Application example

The solution

After a thorough analysis of the application requirements, Rollon Nadella engineers proposed the AXNRQ circular system in-ring configuration. This solution was selected due to its ability to meet the key operational demands of the project, offering:

  • High load capacity with robust guide rollers that support loads in all directions, helping ensure smooth and stable transportation of coils.
  • Optimized acceleration and speed, meeting the stringent stroke time requirement between machine stations.
  • Space-efficient design, allowing seamless integration onto the existing 10-meter-long support structure within the plant.

The system provided features a 10-meter-long circular track equipped with 24 carriages, ensuring continuous operation across all machining stations.

Built to handle automated wire products, the system features a 10-meter-long circular track with 24 carriages, enabling nonstop operation across all machining stations.

Furthermore, to enhance reliability and minimize maintenance efforts, the solution includes an automatic lubrication system that helps ensure optimal performance over extended operational cycles.

10-meter-long AXNRQ Circular System

The AXNRQ circular system supports the electric wire production process with a fully integrated, ready-to-use circuit that allows manufacturers to achieve the desired performance while reducing footprint and engineering time. The core components of the system include:

  • Aluminum base for lightweight strength and easy installation.
  • Guide rails and carriages for precise and smooth movement.
  • Transmission system with gearbox and toothed belt for efficient motion control.
  • Lubrication units for extended durability and reduced maintenance.
  • Carriage indexing system to ensure accurate positioning at each processing station.

This setup was ideal for a facility focused on electrical wire manufacture, where cycle time and accuracy are key drivers of success.

The automatic lubrication system

The drive pulley directly mounted on the gearbox output shaft

The results

The implementation of the AXNRQ circular system has brought several benefits to the customer’s production process:

  • Improved motion control: the guide rollers enable stable, precise movement, essential for positioning coils accurately during the electric wire manufacturing process.
  • Efficient use of space: The machined aluminum alloy base, directly connected to the gearbox, supports a compact and easy-to-install system.
  • Adaptability to specific needs: The modular and configurable design allows customization for various production setups, helping reduce installation time and engineering workload.

By adopting Rollon Nadella’s AXNRQ circular system, the company was able to implement an automation solution that aligns with its operational requirements, supporting efficiency and productivity improvements while optimizing the use of available space.

This project showed just how effective a custom-built system can be when you’re dealing with the demands of a complex electric wire production process. It met tight timing requirements, worked within limited space, and delivered consistent performance—exactly what the customer needed.

If you’re thinking about upgrading your electric wire manufacturing process, Rollon’s engineering-focused approach gives you a reliable, flexible solution. Whether you’re trying to make your current setup more efficient or looking into newer, more advanced wire products, the right automation system can make a real difference.

For more information on Rollon’s linear motion solutions and to connect with Rollon application engineers in your area or region, please get in touch with us.

Get in touch with us

Related product line

Select a product to learn more

AXNR - Circular System

AXNR Circular System

1
AXNR circular system is composed of groups of standard elements: aluminium basement, guide rails and carriages, transmission by gearbox and toothed belt, lubrication units and carriage indexing for precise carriage location.

Solutions by Industries

  • All
  • Industrial Machines
  • Railway
  • Packaging and Logistics
  • Aerospace
  • Building and Furniture
  • Special Vehicles
  • Medical
  • Integrators
  • Robotics
  • Automotive
  • Electronics
  • Textile
  • Material handling
  • Robotics & Automation
  • Machine Tool
  • Food & Beverage
Blog Post Rollon’s Modular RTU: Built for Flexibility, Delivered in Weeks, Made in the USA
White paper Applying Linear Motion Components in Tertiary Packaging Machinery
Tech Talks Understanding Axial vs. Radial Loads in Linear Guides
Blog Post How to Choose a Rod End: A Technical Guide for Design Engineers
Case Study How Rollon’s Compact Rail Enhanced Visibility on Maintenance Locomotive
Case Study Rollon Precision System Solution Helps JR Automation Deliver Increased Medical Device Assembly Speed
Blog Post How to Choose a Rod End: A Technical Guide for Design Engineers
White paper The Critical Role of Linear Motion Solutions in Industrial Machinery
White paper Applications For Industrial Grade Telescopic Rails
Tech Talks Where to Use Wall-Mounted RTU's
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Tech Talks Factors to Consider When Selecting and Integrating an RTU
Case Study How Rollon’s Compact Rail Enhanced Visibility on Maintenance Locomotive
Tech Talks Where to Use Wall-Mounted RTU's
Tech Talks E-Smart and R-Smart actuators in logistics, material handling, automation, and robotics
Tech Talks When to Preload Linear Guides and Actuators (and when not to)
Tech Talks Misalignment & Cost of Ownership
Tech Talks Choosing Between Telescopic Rails with I-beam Assemblies and S-shaped Frames
White paper Applying Linear Motion Components in Tertiary Packaging Machinery
Blog Post How to Choose a Rod End: A Technical Guide for Design Engineers
White paper Linear motion in robotics and automation: Overview and trends
Tech Talks Where to Use Wall-Mounted RTU's
Case Study Rod Ends for Material Handling
Tech Talks E-Smart and R-Smart actuators in logistics, material handling, automation, and robotics
Tech Talks Cleanroom-Ready Linear Motion, Engineered for Precision
Tech Talks Where to Use Wall-Mounted RTU's
Tech Talks Misalignment & Cost of Ownership
Tech Talks Choosing Between Telescopic Rails with I-beam Assemblies and S-shaped Frames
Blog Post Why EN 9100 Certification is Important
Blog Post Choosing Between Robotics and Multi-Axis Cartesian Systems
Tech Talks Where to Use Wall-Mounted RTU's
White paper Preventing Corrosion with Stainless-steel and other Motion Components
Tech Talks Misalignment & Cost of Ownership
Tech Talks Choosing Between Telescopic Rails with I-beam Assemblies and S-shaped Frames
Tech Talks How to Select and Combine T, U, and K Compact Rail Components
Blog Post This Adaptive Linear Rail Provides Demanding Industries With Many Benefits
Tech Talks Where to Use Wall-Mounted RTU's
White paper Preventing Corrosion with Stainless-steel and other Motion Components
Case Study Rod Ends for Agricultural Machines
Tech Talks E-Smart and R-Smart actuators in logistics, material handling, automation, and robotics
Case Study Pre-assembled and custom motorcycle components
Tech Talks When to Preload Linear Guides and Actuators (and when not to)
Case Study Rollon Precision System Solution Helps JR Automation Deliver Increased Medical Device Assembly Speed
Tech Talks Rosa Sistemi Needle Roller and Cross Roller Guides – Explained by Rollon Experts
White paper Linear motion in robotics and automation: Overview and trends
Tech Talks Cleanroom-Ready Linear Motion, Engineered for Precision
White paper Applications For Industrial Grade Telescopic Rails
Tech Talks Where to Use Wall-Mounted RTU's
Tech Talks Where to Use Wall-Mounted RTU's
Tech Talks Factors to Consider When Selecting and Integrating an RTU
Tech Talks How Rollon’s Curvilinear Transfer Systems Outperform Other Transfer Systems
Blog Post Monorail linear guide for high-load applications
Tech Talks E-Smart and R-Smart actuators in logistics, material handling, automation, and robotics
Blog Post Where to Use Wall-Mounted Robot Transfer Units
White paper Applications For Industrial Grade Telescopic Rails
Tech Talks Where to Use Wall-Mounted RTU's
Tech Talks E-Smart and R-Smart actuators in logistics, material handling, automation, and robotics
Tech Talks When to Preload Linear Guides and Actuators (and when not to)
Tech Talks Misalignment & Cost of Ownership
Tech Talks Choosing Between Telescopic Rails with I-beam Assemblies and S-shaped Frames
Case Study Pre-assembled and custom motorcycle components
Case Study How Rollon Actuators Helped a Korean Multinational Corporation Automate its Battery Cell Manufacturing Process
Tech Talks Cleanroom-Ready Linear Motion, Engineered for Precision
Case Study High-Tech Distributor Taps Rollon for Electronics Machine
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Blog Post Monorail linear guide for high-load applications
Case Study Moving Printing Machinery in the Textile Industry with Compact Rail Plus
Blog Post How to Choose a Rod End: A Technical Guide for Design Engineers
White paper Linear motion in robotics and automation: Overview and trends
Tech Talks Cleanroom-Ready Linear Motion, Engineered for Precision
Case Study Automating the electric wire production process
Case Study High-Tech Distributor Taps Rollon for Electronics Machine
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Tech Talks Factors to Consider When Selecting and Integrating an RTU
Tech Talks Rosa Sistemi Needle Roller and Cross Roller Guides – Explained by Rollon Experts
White paper Differences between ball screws for heavy equipment, automation, and machine tools
Tech Talks Factors to Consider When Selecting and Integrating an RTU
Blog Post Monorail linear guide for high-load applications
Blog Post Where to Use Wall-Mounted Robot Transfer Units
Tech Talks Misalignment & Cost of Ownership
White paper Preventing Corrosion with Stainless-steel and other Motion Components
Blog Post Rollon Linear Motion Solutions for Vertical Farming
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
      • Needle Bearings
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
cz-flagČesko fr-flagFrance de-flagDeutschland it-flagItalia nl-flagNederland pl-flagPolska pt-flagPortugal es-flagEspaña gb-flagUnited Kingdom sw-flagSweden/Nordics

Asia

cn-flag中国 in-flagIndia jp-flag日本 kr-flag한국 tr-flagTürkiye

America

br-flagBrasil us-flagUnited States

Ask Rollon

Our Experts can solve your challenges